What is the state of the GPIO of the STM32F767ZIT6 during reset and after reset before configuration?
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-11-15 3:55 PM
The notes in the STM32F76xxx data sheet DS11532 Rev 7 give 2 different answers to this question. See attached. I'm guessing the default state of the unconfigured GPIO is "Floating Input."
Labels:
- Labels:
-
Documentation
-
GPIO-EXTI
-
RESET
-
STM32F7 Series
1 REPLY 1
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-11-15 7:50 PM
There are a couple of exceptions, as noted by the register initialization values,but yes mostly input/floating. ie transistors both off, pull up/down resistors not connected.
Analogue Input would be where the digital schmitt trigger on the input is disabled, so nothing internally is going to react to a perceived potential change on the pin itself
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Up vote any posts that you find helpful, it shows what's working..