Skip to main content
Associate III
Jun 11, 2024 1:52 PM UTC
Solved

what is the smallest achievable delay in microseconds for a 16-bit and a 32-bit timer?

Hi, I want to generate a 1 microsecond (1 µs) timer interrupt on the STM32G0B1RCT6 microcontroller using its internal clock(16MHz). I am currently using a 16-bit timer to achieve a 5 microsecond delay, but I cannot achieve a 1 microsecond delay. My question is: what is the smallest achievable delay in microseconds for a 16-bit and a 32-bit timer?

This topic has been closed for replies.
Tesla DeLorean
Tesla DeLoreanBest answer
Guru
Jun 11, 2024 2:42 PM UTC

This was already explained too you. You can't interrupt at this rate, you basically saturate the processors with busy work, and nothing gets done.

What you can do is have a maximal counter, running as fast as the processor clock, so whatever quantum that factors out at.

ie TIM->PSC = 0, TIM->ARR=0xFFFF

For a TIM clock running at 48 MHz, TIM->CNT increments every 20.833 ns

uint16_t start = TIM1->CNT;

while((TIM1->CNT - start) < 48); // 1us at 48 MHZ

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..

3 replies

Andrew Neil
Super User
Jun 11, 2024 2:30 PM UTC

You've already got a thread on this:

https://community.st.com/t5/stm32-mcus-boards-and-hardware/how-to-generate-a-1-microsecond-1-%C2%B5s-timer-interrupt-on-the/m-p/684321#M19430

 


@Berlin-raj123 wrote:

Hi, I want to generate a 1 microsecond (1 µs) timer interrupt 


In that thread, several people have already asked you why you feel the need to do that, and have explained that it's a Bad Idea.

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Tesla DeLorean
Tesla DeLoreanBest answer
Guru
Jun 11, 2024 2:42 PM UTC

This was already explained too you. You can't interrupt at this rate, you basically saturate the processors with busy work, and nothing gets done.

What you can do is have a maximal counter, running as fast as the processor clock, so whatever quantum that factors out at.

ie TIM->PSC = 0, TIM->ARR=0xFFFF

For a TIM clock running at 48 MHz, TIM->CNT increments every 20.833 ns

uint16_t start = TIM1->CNT;

while((TIM1->CNT - start) < 48); // 1us at 48 MHZ

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
mƎALLEm
ST Technical Moderator
Jun 11, 2024 2:49 PM UTC

Hello @Berlin-raj123 

Could you please tell why are you duplicating this thread from https://community.st.com/t5/stm32-mcus-boards-and-hardware/how-to-generate-a-1-microsecond-1-%C2%B5s-timer-interrupt-on-the/m-p/684321#M19430 ?

Are all these answers didn't convince you?

I agree with @Tesla DeLorean you will saturate the processor at this rate for nothing as you didn't explain the main reason for doing that!

Otherwise the thread will be closed.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.