2020-08-24 03:49 AM
On H7 MCU, waht is the minimum freq of SCK on SPI block? I try to connect a ADC with max SCK 3.2Mhz to H7's SPI port.
2020-08-24 06:34 AM
For master, it'll depend on your clock settings. you can max out the prescaler and set the input clock as low as possible.
You shouldn't have a problem getting it below 3.2MHz regardless of clock settings.