2021-05-12 06:42 PM
For example, What does 'Z' and 'I' mean in Nucleo-F767ZI and what does 'Z' and 'G' mean in Nucleo-F767ZG?
In this way, please tell me the meaning of the things that are divided into R, E, B, K, C, etc.
2021-05-12 07:52 PM
The Nucleo-F767ZI has an STM32F767ZI chip. The Z means it's an 144 pin package and the I means it has 2MB of FLASH. See the datasheet for specifics.
https://www.st.com/resource/en/datasheet/stm32f767zi.pdf
The Nucleo-F767ZG doesn't exist, but the NUCLEO-F746ZG has an STM32F746ZG chip. The G means it has 1MB of FLASH.
2021-05-17 02:49 AM
Hello @Lsang.1,
You can refer to the Ordering information section in datasheet , you will find all the information of each alphabet.
Mohamed Aymen.