cancel
Showing results for 
Search instead for 
Did you mean: 

What is the maximum input voltage for the external voltage regulator of the stm32 bluepill?

HAbay.1
Associate III

I am referring to the regulator connected to the usb 5V ( the 5V pin), can it handle a voltage of 12v and step it down to 3.3V for the chip? if not then what is the limit?

1 ACCEPTED SOLUTION

Accepted Solutions

Check the schematic and placed components on the board you have

RT9193-33 looks to max out at 5.5V

https://www.richtek.com/assets/product_file/RT9193/DS9193-16.pdf

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

View solution in original post

2 REPLIES 2

Check the schematic and placed components on the board you have

RT9193-33 looks to max out at 5.5V

https://www.richtek.com/assets/product_file/RT9193/DS9193-16.pdf

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Uwe Bonnes
Principal III

Bluepill is produced by many asian companies. Parts used may differ, but assuming 5.5 V max is a good guess.