‎2020-04-16 10:54 PM
Is it possible to drive the controller with 480 MHz and therefor the flash with 240 MHz?
How many waitstates have to be set at 240 MHz?
‎2020-04-16 11:42 PM
Look for FLASH recommended number of wait states in the reference manual.
‎2020-04-17 1:52 AM
In Table 13 in reference manual (DS12110 Rev 7) the maximum frequency is 225 MHz (see attachment). But in Comment (1) there is a reference to the maximum product Faclk frequency (240 MHz).
If I config the Faclk freqency to 240 MHz in the STM32CubeMx there is no error and the controller is running well.
‎2020-04-17 2:41 AM
Can you double-check you're looking at the right document.
For stm32H743, the Reference Manual is RM0433 for "STM32H742, STM32H743/753 and STM32H750 Value line
advanced Arm®-based 32-bit MCUs"
And that states in Table 17 that you need to be in VOS0 to go to 240 MHz.
‎2020-04-17 2:54 AM
> Reference Manual is RM0433
and Revision 7 dated Feb 27, 2020
‎2020-04-17 2:55 AM
Thank you. I've got the wrong version :face_with_tears_of_joy: