cancel
Showing results for 
Search instead for 
Did you mean: 

What is the frequency shift by temperature of STM32L0xx MSI(Multi-Speed Internal)?

E-John
Associate III

"The operating temperature has an impact on the accuracy of the RC oscillators. At 25 °C, the HSI16 oscillator has an accuracy of ±1% typically, the MSI oscillator has an accuracy of ± 0.5% and the HSI48 oscillator has an accuracy of ±4%."

It is described on page 1 of AN4631 How to calibrate an STM32L0xx internal RC oscillator.

One of the Ceramic Resonator(HSE ) has Frequency Shift by Temperature +/-0.20% max.

Frequency Tolerance +/-0.50% max.

Operating Temperature Range - ℃ 20 to ℃ 

Just want to know what is the frequency shift by temperature for STM32L0xx MSI(Multi-Speed Internal)?

Thanks and Best regards,

E-John

1 ACCEPTED SOLUTION

Accepted Solutions
Danish1
Lead III

This sort of thing would normally be in the data sheet for your stm32 (unless it is so new this has not been characterised)

For example stm32l031 data sheet Rev 4* has in the "Electrical Characteristics" "Operating Conditions" "Internal Clock Source Characteristics" a table on "MSI Oscillator Characteristics" - Table 43 on pages 72-73

It says the MSI might vary by 3% over temperature, and 2.5%/V over supply-voltage.

Don't rely on these variations to be linear. Chip designers use a lot of "tricks" to eliminate variations as best they can (for example current sources that are "PTAT" (proportional to absolute temperature).

Hope this helps,

Danish

*Possibly not the most recent but that's the one I downloaded when looking at this chip to see if it was the right one for a particular project, so the table or page numbers might have changed

View solution in original post

2 REPLIES 2
Danish1
Lead III

This sort of thing would normally be in the data sheet for your stm32 (unless it is so new this has not been characterised)

For example stm32l031 data sheet Rev 4* has in the "Electrical Characteristics" "Operating Conditions" "Internal Clock Source Characteristics" a table on "MSI Oscillator Characteristics" - Table 43 on pages 72-73

It says the MSI might vary by 3% over temperature, and 2.5%/V over supply-voltage.

Don't rely on these variations to be linear. Chip designers use a lot of "tricks" to eliminate variations as best they can (for example current sources that are "PTAT" (proportional to absolute temperature).

Hope this helps,

Danish

*Possibly not the most recent but that's the one I downloaded when looking at this chip to see if it was the right one for a particular project, so the table or page numbers might have changed

Ozone
Lead II

Never heard of a "Multi-Speed Internal" oscillator, it seems new with this part - or family.

As you cited the tolerances of other oscillators, I suppose this specific one is missing from the datasheet.

Mistakes happen, so I would inquire ST directly. An perhaps ask for an updated datasheet.