cancel
Showing results for 
Search instead for 
Did you mean: 

What is the correct connection for VCAP1 and VCAP2?

exlabs
Associate II

Hello,

VCAP1 and VCAP2 are external capacitors for the core's voltage regulator.

The data sheet for the STM32F479VI states that, "Stabilization for the main regulator is achieved by connecting an external capacitor CEXT to the VCAP1/VCAP2 pins."

I interpret this as a series connection, like this,

Screenshot 2024-08-07 at 16.33.18.png

Table 19 gives some more information,

exlabs_0-1723045268783.png

It mentions "the two 2.2uF Vcap capacitors...", are they bypass capacitors that need to connect to ground, one for each pin? I looked around online and found people using this scheme,

 

Screenshot 2024-08-07 at 16.33.45.png

  1. Which scheme is correct?
  2. Should I adjust the total capacitance to be 2.2u for the second scheme i.e 2 x 4.7uF would be OK?
  3. Using two capacitors (as above) would decouple RF and half the ESR, which are both useful.

Regards,

 

1 ACCEPTED SOLUTION

Accepted Solutions
Andrew Neil
Evangelist III

AndrewNeil_0-1723046019080.png

AndrewNeil_1-1723046043544.png

 

 

See also AN4488Getting started with STM32F4xxxx MCU hardware development

View solution in original post

1 REPLY 1
Andrew Neil
Evangelist III

AndrewNeil_0-1723046019080.png

AndrewNeil_1-1723046043544.png

 

 

See also AN4488Getting started with STM32F4xxxx MCU hardware development