cancel
Showing results for 
Search instead for 
Did you mean: 

What happened to Arduino Star Otto?

Posted on December 22, 2016 at 21:00

0690X00000603XWQAY.jpg

http://www.st.com/en/evaluation-tools/ard-otto-stmhtml

http://www.st.com/content/st_com/en/about/media-center/press-item.html/t38html

#arduino

Note: this post was migrated and contained many threaded conversations, some content may be missing.
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
33 REPLIES 33
LMI2
Lead
Posted on February 15, 2017 at 15:16

Is there a schematic for this?

Posted on February 15, 2017 at 17:32

It is supposedly 'Open' so may be you should be asking Arduino directly?

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Posted on February 15, 2017 at 17:38

http://www.arduino.org/forums/star/info-about-arduino-star-otto-817

 

http://www.arduino.org/forums/star/schematic-of-the-star-otto-773

 
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Posted on February 15, 2017 at 21:44

I am quite surprised how urging the requests are, in light of abundance of various Pies and similar.

Can you or anybody else please enlighten me, what's the point I am obviously missing?

JW

Posted on February 15, 2017 at 22:55

I guess there is some frustration in that it was announced over a year ago, as part of ST's strategy to take Arduino focus away from Atmel

It would be one of the first with the Arduino Mega foot-print with more IO and USART access, and MicroSD card slot.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Posted on February 15, 2017 at 23:26

A more capable/powerful/modern microcontroller, but still inside the Arduino framework.

Some people value familiarity and are ready to pay, I can only assume, a steeper price than what they would pay for the STM's discovery boards.
Posted on February 15, 2017 at 23:42

Clive One wrote:

I guess there is some frustration in that it was announced over a year ago, as part of ST's strategy to take Arduino focus away from Atmel

+1 Arudino had also an internal power struggle... U

nfortunately,

that board/project has probably been created sometime in early 2015 and has been waiting since then.

It would be one of the first with the Arduino Mega foot-print with more IO and USART access, and MicroSD card slot.

+ on board SDRAM, Camera interface, DSI-MIPI and WiFi.

Posted on February 16, 2017 at 00:10

Well, well then... I am curious how will this board do when it finally appears.

JW

Posted on February 16, 2017 at 13:03

Me too  It all depends on the price, if they price it significantly higher than 50-60$ they will probably experience bad sales numbers.

The new H7 discovery boards that are coming out soon will probably have the same price tag...
Posted on February 16, 2017 at 14:46

It all depends on the price, if they price it significantly higher than 50-60$ they will probably experience bad sales numbers.

That would be already about 150% of a Raspberry PI, Odroid C1 or similar Cortex A board. I would prefer another one of those ...

The new H7 discovery boards that are coming out soon will probably have the same price tag...

I'd rather have a version without GPIO pins tied up in stuff of dubious usability like LCD displays, MEMS sensors or audio amplifiers.I prefer to have that as optional add-on board (like the TI Tiva Launchpads with their 'booster boards').

Or alternatively, as H7 Nucleo board.