2016-12-22 12:00 PM
http://www.st.com/en/evaluation-tools/ard-otto-stmhtml
http://www.st.com/content/st_com/en/about/media-center/press-item.html/t38html
#arduino Note: this post was migrated and contained many threaded conversations, some content may be missing.2017-02-15 6:16 AM
Is there a schematic for this?
2017-02-15 9:32 AM
It is supposedly 'Open' so may be you should be asking Arduino directly?
2017-02-15 9:38 AM
http://www.arduino.org/forums/star/info-about-arduino-star-otto-817
http://www.arduino.org/forums/star/schematic-of-the-star-otto-773
2017-02-15 12:44 PM
I am quite surprised how urging the requests are, in light of abundance of various Pies and similar.
Can you or anybody else please enlighten me, what's the point I am obviously missing?
JW
2017-02-15 2:55 PM
I guess there is some frustration in that it was announced over a year ago, as part of ST's strategy to take Arduino focus away from Atmel
It would be one of the first with the Arduino Mega foot-print with more IO and USART access, and MicroSD card slot.
2017-02-15 3:26 PM
A more capable/powerful/modern microcontroller, but still inside the Arduino framework.
Some people value familiarity and are ready to pay, I can only assume, a steeper price than what they would pay for the STM's discovery boards.2017-02-15 3:42 PM
Clive One wrote:
I guess there is some frustration in that it was announced over a year ago, as part of ST's strategy to take Arduino focus away from Atmel
+1 Arudino had also an internal power struggle... U
nfortunately,
that board/project has probably been created sometime in early 2015 and has been waiting since then.
It would be one of the first with the Arduino Mega foot-print with more IO and USART access, and MicroSD card slot.
+ on board SDRAM, Camera interface, DSI-MIPI and WiFi.
2017-02-15 4:10 PM
Well, well then... I am curious how will this board do when it finally appears.
JW
2017-02-16 5:03 AM
Me too It all depends on the price, if they price it significantly higher than 50-60$ they will probably experience bad sales numbers.
The new H7 discovery boards that are coming out soon will probably have the same price tag...2017-02-16 6:46 AM
It all depends on the price, if they price it significantly higher than 50-60$ they will probably experience bad sales numbers.
That would be already about 150% of a Raspberry PI, Odroid C1 or similar Cortex A board. I would prefer another one of those ...
The new H7 discovery boards that are coming out soon will probably have the same price tag...
I'd rather have a version without GPIO pins tied up in stuff of dubious usability like LCD displays, MEMS sensors or audio amplifiers.I prefer to have that as optional add-on board (like the TI Tiva Launchpads with their 'booster boards').
Or alternatively, as H7 Nucleo board.