cancel
Showing results for 
Search instead for 
Did you mean: 

What does 'Value Line' stand for? What is the difference to the 'non Value Line' devices?

Led
Senior

Several MCU are described with the label 'value line' but I could not find an explanation what that mean. I assume it is related to a system architecture, right?

1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

With the Value line, individual functions were measured with looser tolerances or were completely omitted for reasons of cost. If you compare the data sheets of the Value Line with those of the Access Line, you can see very quickly which parameters are affected. Sometimes it is the voltage range, sometimes the missing serial number, or other parameters.

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
Peter BENSCH
ST Employee

With the Value line, individual functions were measured with looser tolerances or were completely omitted for reasons of cost. If you compare the data sheets of the Value Line with those of the Access Line, you can see very quickly which parameters are affected. Sometimes it is the voltage range, sometimes the missing serial number, or other parameters.

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Thank you very much for the fast answer.

Led