cancel
Showing results for 
Search instead for 
Did you mean: 

vref voltage of stm32f429 disc1

harry123
Senior II

Hello all. I am working with internal ADC can I know what is the internal reference voltage and how to change the internal reference voltage? 

1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

You can find this information in the STM32F429ZI data sheet, section 6.3.24:

VREFINT (Internal reference voltage) = min 1.18V, typ 1.21V, max 1.24V

You cannot change it, but you could apply an external reference voltage to VREF+ (pin 32) if you first desolder R58, which connects VREF+ to VDD.

Hope that helps?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

4 REPLIES 4
Peter BENSCH
ST Employee

You can find this information in the STM32F429ZI data sheet, section 6.3.24:

VREFINT (Internal reference voltage) = min 1.18V, typ 1.21V, max 1.24V

You cannot change it, but you could apply an external reference voltage to VREF+ (pin 32) if you first desolder R58, which connects VREF+ to VDD.

Hope that helps?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Thank you ...but there is an option to change VDD in cubemx tried it but the result looks the same.

waclawek.jan
Super User

> but there is an option to change VDD in cubemx

Where exactly?

JW

> but there is an option to change VDD in cubemx

Do you mean VDD in the RCC, System Parameters block?

This has no effect on a reference voltage, but on a #define VDD_VALUE, for example, which can be used for ratiometric measurements, among other things. A reference voltage is generally independent of the supply voltage - otherwise it would not be a reference, would it?

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.