cancel
Showing results for 
Search instead for 
Did you mean: 

VREF Internal voltage reference G431 series

CrazyChel
Associate III

Hello,

Can anyone suggest whether or not I need to connect external capacitors to the VREF+ pin if I plan to use VREF only for the onboard DAC?
Could this be a hardware problem?
STM32G431CBT6. The problem is that on the oscillogram I see oscillations with an amplitude of approximately 490 mV on the VREF+ pin. This is when Scale 2 is set to 2.9 V. If I reduce to 2.5V, the swing will be almost 1V overall. Nothing but the 1:10 oscilloscope probe is connected to the VREF+ pin on the board.
Below are the screenshots.

Settings.png

Oscillogram.png

Pinout.png

Capacitors.png

1 ACCEPTED SOLUTION

Accepted Solutions
TDK
Guru

Yes, it needs capacitors if you are using the DAC, per the datasheet and the hardware design guide.

If you feel a post has answered your question, please click "Accept as Solution".

View solution in original post

4 REPLIES 4
TDK
Guru

Yes, it needs capacitors if you are using the DAC, per the datasheet and the hardware design guide.

If you feel a post has answered your question, please click "Accept as Solution".

Thank you! The question is closed.
I have already connected 0.1 µF and 20 pF. Now I can switch between different ref values.

> I have already connected 0.1 µF and 20 pF.

I don't think these are the values required by the datasheet.

JW

Thank you, I also noticed that this is not enough, I will increase it.