2018-11-12 7:22 AM
Hi
My stm32l433cc circuit has two different LDO, one for Vdd and another for Vdda. Can you tell
me please can i run my controller without Vdda power? I need to turn on/off analog power
when i need it. Is it possible on stm32l433cc?
2018-11-12 7:42 AM
What does the datasheet say, in the General operating conditions table, for VDDA?
JW
PS. There are requirements for ramp-up/ramp-down when VDD and VDDA are separate. Also, lower VDDA will impact the 5V-tolerance of pins connected to analog peripherals, see VINmax for IO pins. There may be other similar effects; read the datasheet.
2018-11-12 8:22 AM
Stm32f030 datasheet says Vdda "Must have a potential equal to or higher than VDD", but i got none the same about stm32l433.
So, i can use two separate LDOs?
2018-11-12 8:29 AM
Look at other block diagrams, typically the PLL and reset stuff is in the analogue domain.
2018-11-12 8:31 AM
Datasheet says "Reset block, Temp. sensor, PLL, HSI, MSI, HSI48" is Vdd Domain
2018-11-12 8:33 AM
The STM32L433 Datasheet says this, take it for what it's worth..
"The VDDA voltage level is independent from the VDD voltage."