2024-06-09 11:18 PM - edited 2024-06-09 11:19 PM
Hello forum!
I'm struggling to enable the burst feature described in the applicationnote from stm.
I'm using cube IDE and I configured timer1 along with DMA1 to generate a specific waveform.
Problem is, that after enabling the PWM via "HAL_TIM_PWM_START_DMA()",
the call to HAL_TIM_DMAburst_Multiwrite() failes with HAL_BUSY.
The initial values are set but the update does not work. Are there any experiences to use
this feature using cubeIDE (Cubemx)?
Solved! Go to Solution.
2024-08-06 02:11 AM
Hello @Bertl, welcome to ST Community, sorry for the delayed answer!
Could you specify what stm32 are you using?
You can start from the existent cube example of TIM_DMABurst here.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-08-06 02:11 AM
Hello @Bertl, welcome to ST Community, sorry for the delayed answer!
Could you specify what stm32 are you using?
You can start from the existent cube example of TIM_DMABurst here.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-08-06 04:47 AM
Hi, thanks for the answer!
Meanwhile, I managed to get it work 🙂