2024-10-16 07:25 AM
hello
I am developping on a STM32G0B0RE, I've learned after finishing my board and everything that boot pin can be used by default.
It is not a problem since I have ST-Link for production but I would like to be able to do firmware update through bootloader.
The issue is, since nBOOT_SEL is set to '1' by default I need to change it to 0 so I go in bootloader if my pin PA14-BOOT0 is tied up at startup. I find how to change it in STM32CubeProgrammer but I would like to do it in my firmware so the flashing process is not too complicated in factory.
I've tried this but it does not have any effect :
Best Regards
Thibaud HABRAND
2024-10-16 09:08 AM