cancel
Showing results for 
Search instead for 
Did you mean: 

Using BC1.2 in STM32G473CE

PY.1
Associate II

Hi,

I want to use BC1.2 protocol of STM32G473CE MCU. But STM32G473CE supports USB PD also. So in order to use only BC1.2 can I use only Dp Dm lines of STM32G473CE and leave CC lines un-connected

Also what is the maximum power negotiation performed by STM32G473CE when using BC1.2 protocol?

1 REPLY 1
FBL
ST Employee

Hello @PY.1 

If you would like to use USB 2.0 legacy device to function with a USB Type-C port, you can pull down CC lines to ground as referenced in the figure below extracted from AN5225

FBL_1-1719241615720.png

According to table 3 : Power supply options, in same App note 

FBL_2-1719244984205.png

 

 The maximum power would be 7.5W

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.