User Activity

Hi,We are using STM32G473CEU3 in our designWe have a situation that when MCU is powered off, 3.3V appears on one of the IO pins from an external circuit with 2mA of sourcing. Will this damage the MCU or is it ok?
Hi,I want to use BC1.2 protocol of STM32G473CE MCU. But STM32G473CE supports USB PD also. So in order to use only BC1.2 can I use only Dp Dm lines of STM32G473CE and leave CC lines un-connectedAlso what is the maximum power negotiation performed by S...
Hi,I'm looking for  USB type C PD controller IC.We need 3 USB type C ports in our design. 1st port should support dedicated power in (up to 140W) and the 2nd and 3rd port should be dedicated for power out (65W) with variable power outThe product oper...
Hi sir/madam,In the datasheet of STM32H750XB 57th page J1 pin name is given as PH0-OSC-OUT and in 61st page the same pin is given as PH1-OSC-OUT. which do we need to consider?Datasheet: https://www.st.com/resource/en/datasheet/stm32h750ib.pdf 
Hi, We are designing a USB 2.0 interface between STM32H750IB and PC.PC will be acting as Host and STM32H750IB will be acting as Device.But for some reasons like future upgradability, we are using USB Type-C Connector.Note that we are going to use USB...
Kudos from