cancel
Showing results for 
Search instead for 
Did you mean: 

Use STM32F4 flash for non-volatile data storage (eeprom)

syedhashmiraza
Associate II

hello i am using stm32f429i-disc1 microcontroller in this how to generate flash code (eeprom)

22 REPLIES 22

This code is not build on stm32f429i-disc1 and iam using stm32cube ide software

What do you mean?

AndrewNeil_0-1731674288942.png

 

when i build this so many error are showing ?

syedhashmiraza
Associate II

(merged from duplicate thread)

 

hello iam using srm32f429i-disc1 microcontroller and i want refrence code for emulated eeprom 

I think you have to use the STM32 HAL library. 

yes iam using HAL library

hello iam using srm32f429i-disc1 microcontroller and i want refrence code for emulated eeprom 

this code is not build in stm32cubeide

syedhashmiraza_0-1731748623361.png

 

The EEPROM emulation itself is just the eeprom.c & eeprom.h files.

The rest is just a "test harness" to demonstrate that.

So you should be able to:

  1. Create a new Project in CubeIDE - make sure that builds as-is.
  2. Copy the  eeprom.c & eeprom.h files into your project.
  3. Copy the test code as text from main.c in the EEPROM GitHub, and paste it into the main.c in your own project.
syedhashmiraza
Associate II

Hello,

I want to read and write string in eeprom  this is my code but in this code string is not storing in eeprom

 

#include "main.h"
#include <stdio.h>

/** @addtogroup EEPROM_Emulation
* @{
*/


/* Private typedef -----------------------------------------------------------*/
/* Private define ------------------------------------------------------------*/
/* Private macro -------------------------------------------------------------*/
/* Private variables ---------------------------------------------------------*/


/* Virtual address defined by the user: 0xFFFF value is prohibited */

uint16_t VirtAddVarTab[NB_OF_VAR] = {0x5555, 0x6666, 0x7777};

uint16_t VarDataTab[NB_OF_VAR] = {0, 0, 0};

uint16_t VarValue,VarDataTmp = 0;

/* Private function prototypes -----------------------------------------------*/
static void SystemClock_Config(void);
static void Error_Handler(void);

/* Private functions ---------------------------------------------------------*/

/**
* @brief Main program.
*  None
* @retval None
*/

//char writeString[] = "Hello Hashmi";
char readString[64]={0};


int main(void)
{
	/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
	HAL_Init();

	/* Configure the system clock to 180 MHz */
	SystemClock_Config();

	/* Unlock the Flash Program Erase controller */
	HAL_FLASH_Unlock();

	/* Configure LED3 */
	BSP_LED_Init(LED3);

	/* EEPROM Init */
	if( EE_Init() != EE_OK)
	{
		Error_Handler();
	}

	if((EE_ReadVariable(VirtAddVarTab[0], &readString[0])) != HAL_OK)
	{
		Error_Handler();
	}
	while(1)
	{
		char writeString[] = "Hello";
		for (int i = 0; i < sizeof(writeString); i++)
		{
			if (EE_WriteVariable(VirtAddVarTab[0] + i, (uint16_t*)&writeString[i]) != HAL_OK)
			{
				Error_Handler();
			}
		}
	}
}