2019-07-08 04:43 PM
hi if it is possible you have an example where I write the value 8 to the eeprom and then I read it again in the same address ...
Hal_FLASH_programm ... (). And read
thank you
2019-07-08 05:24 PM
For what STM32, there are hundreds of them at this point.
There should be FLASH examples under the HAL trees. The memory is readable like any other.
2019-07-09 04:02 AM
Please show me link!
Thanks