2014-04-09 02:11 AM
Hello,
I'm trying to configure SPI1 with NSS software management in my STM32F100, because I want to manage NSS pin as a generic IO pin. Is this possible? For example, I've configured my NSS pin as a generic open-drain and I connected it to 3v3 by a pull-up resistor, but the signal at the pin is always low. This's my configuration: // Enable GPIO clock RCC_APB2PeriphClockCmd( SPI_SCK_GPIO_CLK | SPI_MISO_GPIO_CLK | SPI_MOSI_GPIO_CLK | SPI_NSS_GPIO_CLK | RCC_APB2Periph_AFIO, ENABLE); // Enable SPI clock RCC_APB2PeriphClockCmd(RCC_APB2Periph_SPI, ENABLE); GPIO_InitStructure.GPIO_Pin = SPI_SCK_PIN | SPI_MOSI_PIN; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP; GPIO_Init(SPI_SCK_GPIO_PORT, &GPIO_InitStructure); GPIO_InitStructure.GPIO_Pin = SPI_MISO_PIN; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN_FLOATING; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_Init(SPI_MISO_GPIO_PORT, &GPIO_InitStructure); GPIO_InitStructure.GPIO_Pin = SPI_NSS_PIN; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_Out_OD; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_Init(NSS_GPIO_PORT, &GPIO_InitStructure); Thanks in advance #stm32 #spi