Skip to main content
A Bravos
Associate III
August 15, 2017
Question

Use CubeMX with BlueNRG-2

  • August 15, 2017
  • 2 replies
  • 618 views
Posted on August 15, 2017 at 11:17

Hi.

Is it possible to use cubemx with BlueNRG-2? If yes how? Where to find code examples for this microcontroller, with interest for Bluetooth BLE. 

I want to start exploring this Upc and I needed information

.

Thank you. Bravos

    This topic has been closed for replies.

    2 replies

    Amel NASRI
    ST Technical Moderator
    August 15, 2017
    Posted on August 15, 2017 at 15:28

    Hi

    Bravos.A

    ‌,

    CubeMX is dedicated for STM32 MCUs. What is exactly your requirement here?

    -Amel

    To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.
    A Bravos
    A BravosAuthor
    Associate III
    August 15, 2017
    Posted on August 15, 2017 at 17:10

     ,

     ,

    Hi Amel,

    Thanks for the answer.

    I need to make a low energy application with bluetooth communication and

    work with, some i2c and spi sensor readings, with few gpios and that is

    ultra miniature, to work at 3.3 volts. As I know the CubeMx, because I

    worked with the Discovery board, it would be interesting this aid, to

    bootloader setup.

    I have never worked directly with bluetooth Ic, and so looking for

    information.

    Bravos

    2017-08-15 14:29 GMT+01:00 Amel N <,st-microelectronics@jiveon.com>,:

    STMicroelectronics Community

    <,https://community.st.com/?et=watches.email.thread>,

    Re: Use CubeMX with BlueNRG-2

    reply from Amel N

    <,

    MCUs Forum* - View the full discussion

    <,https://community.st.com/0D70X000006SqoHSAS