2017-08-15 02:17 AM
Hi.
Is it possible to use cubemx with BlueNRG-2? If yes how? Where to find code examples for this microcontroller, with interest for Bluetooth BLE.
I want to start exploring this Upc and I needed information
.Thank you. Bravos
2017-08-15 06:28 AM
Hi
Bravos.A
,CubeMX is dedicated for STM32 MCUs. What is exactly your requirement here?
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2017-08-15 10:10 AM
,
,
Hi Amel,
Thanks for the answer.
I need to make a low energy application with bluetooth communication and
work with, some i2c and spi sensor readings, with few gpios and that is
ultra miniature, to work at 3.3 volts. As I know the CubeMx, because I
worked with the Discovery board, it would be interesting this aid, to
bootloader setup.
I have never worked directly with bluetooth Ic, and so looking for
information.
Bravos
2017-08-15 14:29 GMT+01:00 Amel N <,st-microelectronics@jiveon.com>,:
STMicroelectronics Community
<,https://community.st.com/?et=watches.email.thread>,
Re: Use CubeMX with BlueNRG-2
reply from Amel N
<,
MCUs Forum* - View the full discussion
<,https://community.st.com/0D70X000006SqoHSAS