Skip to main content
Franz.1
Associate III
August 5, 2024
Solved

USBCPD CubeIDE code results in HardFault when GUI_INTERFACE is enabled

So, I followed the following video step by step for a "project with a custom board" (video minute 13:04)

https://www.youtube.com/watch?v=cbdFHmMOMwk

I am working on an STM32G0B1CBT6

The code is generated and can be built, but as soon as I enable the Utilities->GUI_INTERFACE in CubeMX, the generated code results in a Hardfault during initialisation ( to be specific in the in the file Utilities-> GUI_INTERFACE->bsp_gui.c) during execution of the line number 80, that is

 

 

 

 if ((0xFFFFFFFFu != *((uint32_t *)_addr)) && (MagicNumber != *((uint64_t *)_addr)))

 

 

 

Any hints on how to proceed debugging?

Thanks!

This topic has been closed for replies.
TDK
TDKBest answer
August 5, 2024

The STM32G0B1CBT6 chip has 128 kB of flash. Address 0x803F800 is past the end of the flash which is at 0x08020000.

TDK_0-1722869055634.png

"If you feel a post has answered your question, please click ""Accept as Solution""."

7 replies

TDK
August 5, 2024

Ensure that the address at _addr is valid and lies within a readable memory somewhere.

"If you feel a post has answered your question, please click ""Accept as Solution""."
Franz.1
Franz.1Author
Associate III
August 5, 2024

Well, _addr is defined as

 

uint32_t _addr = GUI_FLASH_MAGIC_NUMBER;

 

 

The GUI_FLASH_MAGIC_NUMBER itself comes from 

 

#define GUI_FLASH_MAGIC_NUMBER ADDR_FLASH_LAST_PAGE

 

 

ADDR_FLASH_LAST_PAGE comes from

 

#if defined (FLASH_OPTR_DBANK) || defined(FLASH_DBANK_SUPPORT)
#define INDEX_PAGE ((FLASH_PAGE_NB * 2u) - 1u) /* Index of latest page */
#else
#define INDEX_PAGE (FLASH_PAGE_NB - 1u) /* Index of latest page */
#endif /* FLASH_OPTR_DBANK || FLASH_DBANK_SUPPORT */
#define ADDR_FLASH_LAST_PAGE (FLASH_BASE + (INDEX_PAGE * FLASH_PAGE_SIZE)) /* Base @ of latest page */
#define ADDR_FLASH_PAGE_END (ADDR_FLASH_LAST_PAGE + FLASH_PAGE_SIZE - 1u)

 

 

This comes all from the pregenerated code. The defines in the section above all refer to the respective stm32g0xx_hal_flash.h.  I did not change any of that and it seems correct.

Franz.1
Franz.1Author
Associate III
August 5, 2024

Ooooh, I had a look in the dataheet, but I had interchanged the Letters in CBT6, it is the 'B" in CBT6 that tells the 128kByte. not the 'C' which is the pincount here. Wrong order :face_with_rolling_eyes:

I changed the following define to the start of the last page (i.e. the last 2k of Flash)

#define ADDR_FLASH_LAST_PAGE	0x1F800

At least the hardfault is gone. I would say this is a bug of the code generator. Anyway: Thanks a lot @TDK !

Associate II
August 6, 2025

Just wanted to surface this thread to ST; this bug still exists. @FBL