2016-06-07 2:40 AM
Hello,
my problem should be simple to solve, but due to it's rather undocumented nature I resort on posting it to this forum. When plugging in the STM32F429 board into a pc, it gets detected as flashdrive with around 2 MB space and two files on it (MBED.HTM and DETAILS.TXT). I want to avoid that.Especially because that ''opening folder'' sequence is directly linked to the bootup sequence. That means, if I power the STM32F429 by battery or usb-charger, it's not booting until the folder can open up.I couldn't find any documentation on that issue. It only appears on the new STM32F429 Disco boards.Please Help!2016-06-07 4:06 AM
Download the most current ST-LINK Utilities and update the firmware.
2016-06-07 4:09 AM
Or use the other USB connector that goes to the F429