Skip to main content
Stastny.Petr
Associate III
April 25, 2024
Question

USB project example

  • April 25, 2024
  • 1 reply
  • 1014 views

Hello,

I need very simple communication of my STM32F722RET6 via USB (Full Speed) - I need to send every 10 ms only data of 20 bytes to some program made by C# in Visual Studio. I found some samples of USB communication on GitHub but I was not able to communicate (in best case without making some special drivers) with C# program. Only VCP worked but the program was in contiuous cycle to read COM port. Please can you advice me where I can find some working sample of connection STM32 and program via USB?

Thank you

This topic has been closed for replies.

1 reply

ST Technical Moderator
April 25, 2024

Hi @Stastny.Petr 

 

Here is examples for F722 Nucleo board STM32CubeF7/Projects/STM32F722ZE-Nucleo/Applications/USB_Device at master · STMicroelectronics/STM32CubeF7 · GitHub

In your case, REPORT_COUNT should be at least 0x14 to send 20bytes of data. Make sure to configure your timer to interrupt every 10 ms.

 

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL