2024-08-31 05:45 AM
I'd like to use both of the Synopsis USB controllers on the STM32H743VIT6, one as device, one as host, but to do that I understand that the other USB controller is accessed through the USB HS device, which is disabled because of the use of LTDC.
Currently I have the FS USB device working as switchable dual-role Host/Device.
I don't know why the HS USB controller is disabled by CubeMX, as the pin outs for HS DM+/- are free.
Is there a way to get around this to use both USB controllers and the LTDC?
2024-08-31 07:06 AM
I tried to have LTDC and both USB , no problem to see:
I am on IDE 1.13.1 .