2017-01-11 12:44 AM
Hi, newby here. I recently bought two discovery boards from Conrad.nl.
One with a STM32F100RTB and the other with a STM8S003K3T.
Now I wanted to upgrade the firmware of the integrated ST-LINK modules on the Discovery boards. According to the documentation :
On ST-LINK/V2-1 boards, upgrade firmware to the version V2J28M
On ST-LINK/V2 boards, upgrade firmware to the version V2J28S7.
On ST-LINK boards, upgrade firmware to the version V1J13S4.
But in my case the STM32 board is updated to firmware V1.JS0
And worse, the STM8 board to firmware V1.J0.S4
This version seems to be too old for the ST-LINK Utility.
What am I doing wrong?
Regards,
Wilko Lunenburg
Note: this post was migrated and contained many threaded conversations, some content may be missing.2017-01-11 3:47 AM
Hi
Lunenburg.Wilko
,What is the version of the firmware upgrade application you are using?
Please make sure to use the last one available on ST website: .If you were not using the last version, please remake the upgrade procedure and tell me to which version your firmware is upgraded?
Khouloud.
2017-01-11 5:39 AM
Hello Khouloud,
Yes, I did use the lastest version of the firmware upgrade application. To be absolutely sure, I downloaded the application again via your link. But the results are the same.
Regards,
Wilko
2017-01-12 5:52 AM
Hi Wilko,
Refereing to the technical note
section3:In your case J=13 (this is the most recent version for the STM32 debug interface.)
-> The upgrade was done conveniently: you have got the last version of
STM32 debug interface but the STM8 debug interface is not supported.
Khouloud.
2017-01-12 7:29 AM
Hi Avatar,
I interpret you post that he probably needs to download a separate update for his STM8 board, and the 'SWIM' debug interface.
In the previous post, I was talking about the STM32VLDiscovery (
STM32F100RB MCU) and not the STM8 board.
Khouloud.
2017-01-12 7:49 AM
That might explain the result, but seems not very helpful for the O.P., though.
I interpret you post that he probably needs to download a separate update for his STM8 board, and the 'SWIM' debug interface.
BTW, I would scrap the ST_LINK V1 altogether, it is a complete failure. I rather use newer, external ST-Link V2 board to debug my old VL-Discoveries ...
2017-01-12 8:32 AM
The OP mentioned a STM8S003K3T in his first post. I suppose that one has a SWIM interface, and need a different firmware.
2017-01-12 8:58 AM
Hi,
The OP mentioned a STM8S003K3T in his first post.
And worse, the STM8 board to firmware
V1.J0.S4
For the STM8 board, t
he STLink firmware is also upgraded correctly:STM32 debug interface is not supported on the board)
is the most recent version for the STM8 debug interface.
Khouloud.
2017-01-12 9:17 AM
This is an older version of just the update, you might be able to stage the older unit through this and update to most current from there.
https://drive.google.com/open?id=0B7OY5pub_GfIR2taa1YzWEJtTmM
2017-01-12 9:22 AM
As I recall the updaters contain multiple images, I've attached a link to my mirror of one of the older ones, but have a collection.
Would agree that the V1 is rather sad, and might not be supported by newer drivers/dlls moving forward, I remember having to fight one of my systems back in the day to get things working, but that's been a couple of years ago.