2024-02-12 12:24 PM
Hi,
I have the following board :
NUCLEO-F429ZI
The datasheet says that UART3 is the STLINK UART that can be used over USB.
I configured this UART but when I try to receive anything from the terminal that is connected to the UART com port, I don't see the interrupt being triggered.
The objective is to receive some data over UART3, process it, and send the processed data over UART6.
UART3 init in main.c
/**
* @brief USART3 Initialization Function
* @PAram None
* @retval None
*/
static void MX_USART3_UART_Init(void)
{
/* USER CODE BEGIN USART3_Init 0 */
/* USER CODE END USART3_Init 0 */
/* USER CODE BEGIN USART3_Init 1 */
/* USER CODE END USART3_Init 1 */
huart3.Instance = USART3;
huart3.Init.BaudRate = 115200;
huart3.Init.WordLength = UART_WORDLENGTH_8B;
huart3.Init.StopBits = UART_STOPBITS_1;
huart3.Init.Parity = UART_PARITY_NONE;
huart3.Init.Mode = UART_MODE_TX_RX;
huart3.Init.HwFlowCtl = UART_HWCONTROL_NONE;
huart3.Init.OverSampling = UART_OVERSAMPLING_16;
if (HAL_UART_Init(&huart3) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN USART3_Init 2 */
/* USER CODE END USART3_Init 2 */
}
hal_msp.c
/**
* @brief UART MSP Initialization
* This function configures the hardware resources used in this example
* @PAram huart: UART handle pointer
* @retval None
*/
void HAL_UART_MspInit(UART_HandleTypeDef* huart)
{
GPIO_InitTypeDef GPIO_InitStruct = {0};
if(huart->Instance==USART3)
{
/* USER CODE BEGIN USART3_MspInit 0 */
/* USER CODE END USART3_MspInit 0 */
/* Peripheral clock enable */
__HAL_RCC_USART3_CLK_ENABLE();
__HAL_RCC_GPIOD_CLK_ENABLE();
/**USART3 GPIO Configuration
PD8 ------> USART3_TX
PD9 ------> USART3_RX
*/
GPIO_InitStruct.Pin = STLK_RX_Pin|STLK_TX_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
GPIO_InitStruct.Alternate = GPIO_AF7_USART3;
HAL_GPIO_Init(GPIOD, &GPIO_InitStruct);
/* USART3 interrupt Init */
HAL_NVIC_SetPriority(USART3_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(USART3_IRQn);
/* USER CODE BEGIN USART3_MspInit 1 */
/* USER CODE END USART3_MspInit 1 */
}
else if(huart->Instance==USART6)
{
/* USER CODE BEGIN USART6_MspInit 0 */
/* USER CODE END USART6_MspInit 0 */
/* Peripheral clock enable */
__HAL_RCC_USART6_CLK_ENABLE();
__HAL_RCC_GPIOC_CLK_ENABLE();
/**USART6 GPIO Configuration
PC6 ------> USART6_TX
PC7 ------> USART6_RX
*/
GPIO_InitStruct.Pin = UART6_TX_Pin|UART6_RX_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
GPIO_InitStruct.Alternate = GPIO_AF8_USART6;
HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);
/* USART6 interrupt Init */
HAL_NVIC_SetPriority(USART6_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(USART6_IRQn);
/* USER CODE BEGIN USART6_MspInit 1 */
/* USER CODE END USART6_MspInit 1 */
}
}
Application code :
int main(void)
{
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_USART3_UART_Init();
MX_USART6_UART_Init();
/* USER CODE BEGIN 2 */
// Start receiving data in interrupt mode
// HAL_UART_Receive(&huart3, rx_buffer, sizeof(rx_buffer),HAL_MAX_DELAY);
if(HAL_UART_Receive_IT(&huart3, rx_buffer, sizeof(rx_buffer)) != HAL_OK)
{
Error_Handler();
}
// Transmit some data
// char *message = "Hello World\n";
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
}
/* USER CODE END 3 */
}
Callback to process the received cmd :
// This function is called when data is received
void HAL_UART_RxCpltCallback(UART_HandleTypeDef *huart)
{
if (huart->Instance == USART3)
{
// If data is received from UART3, send it to UART6
// HAL_UART_Transmit(&huart6, rx_buffer, sizeof(rx_buffer), HAL_MAX_DELAY);
if(HAL_UART_Transmit_IT(&huart6, rx_buffer, sizeof(rx_buffer)) != HAL_OK)
{
Error_Handler();
}
// Restart the interrupt reception on UART3
HAL_UART_Receive_IT(&huart3, rx_buffer, sizeof(rx_buffer));
}
}
I don't understand what is the problem.
Please help and ask for any other details.
Solved! Go to Solution.
2024-02-14 6:24 AM
@Pavel A. @Bob S ,
Thanks for the insights.
I changed my strategy in the following ways :
#define BUFFER_SIZE 1
//calling the following inside main()
if(HAL_UART_Receive_IT(&huart3, &parentRx, BUFFER_SIZE) != HAL_OK)
{
Error_Handler();
}
/**
* @brief Callback function called when UART receive is complete.
*
* @param huart Pointer to the UART handle structure.
*/
void HAL_UART_RxCpltCallback(UART_HandleTypeDef *huart)
{
if (huart->Instance == USART3)
{
parentMessageSts = Motor_Cmd_Recieve_IT(parentRx, parentRxBuf,sizeof(parentRxBuf),&parentRxPtr);
if(HAL_UART_Receive_IT(&huart3, &parentRx, BUFFER_SIZE) != HAL_OK)
{
Error_Handler();
}
}
}
// Motor_Cmd_Receive processes the incoming commands and stores it in a cmd buffe to be processed by another function
// This approach seems to be working.
2024-02-12 1:04 PM
Please start from polling mode RX and TX first. Will it work?
HAL_UART_Receive(&huart3,...)
HAL_UART_Transmit(&huart6,...)
2024-02-12 2:26 PM
Hi @Pavel A.,
Thanks for your reply.
I tried it but it also does not seem to be working.
I used HAL_DELAY_MAX in the time interval.
I also tested just the transmission on UART3 using the HAL_Transmit function in the while(1) loop.
I am getting the buffer on a terminal that is connected to this UART.
So not sure why this is happening.
Regards
smaiti
2024-02-12 3:23 PM
How big is rx_buffer? You do realize that you won't see the interrupt until you have received sizeof(rx_buffer) number of bytes, right?
Also, with your original code that uses interrupts, in the callback you start sending from rx_buffer, and then immediately start receiving new data into that same rx_buffer. HAL_UART_Transmit_IT() returns immediately, before the data has been sent.
2024-02-13 12:59 AM
Polling mode HAL_UART_Receive does not call HAL_UART_RxCpltCallback. Just send N characters from the terminal and it should return. If not, there's an electrical problem.
2024-02-14 6:24 AM
@Pavel A. @Bob S ,
Thanks for the insights.
I changed my strategy in the following ways :
#define BUFFER_SIZE 1
//calling the following inside main()
if(HAL_UART_Receive_IT(&huart3, &parentRx, BUFFER_SIZE) != HAL_OK)
{
Error_Handler();
}
/**
* @brief Callback function called when UART receive is complete.
*
* @param huart Pointer to the UART handle structure.
*/
void HAL_UART_RxCpltCallback(UART_HandleTypeDef *huart)
{
if (huart->Instance == USART3)
{
parentMessageSts = Motor_Cmd_Recieve_IT(parentRx, parentRxBuf,sizeof(parentRxBuf),&parentRxPtr);
if(HAL_UART_Receive_IT(&huart3, &parentRx, BUFFER_SIZE) != HAL_OK)
{
Error_Handler();
}
}
}
// Motor_Cmd_Receive processes the incoming commands and stores it in a cmd buffe to be processed by another function
// This approach seems to be working.
2024-02-14 7:01 AM
Here is a similar thread: https://community.st.com/t5/stm32-mcus-products/uart3-can-t-receive-entire-data/td-p/174371