Unable to receive data on SPI, when configuring SPI1 as Master and SPI3 as Slave
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2022-08-12 12:40 PM
Hi,
I want to interface two SPI peripherals on the same STM32H743 nucleo, am configuring SPI1 as Master and other as Slave and connecting them with each other. Am transmitting in polling mode via SPI1 and receiving in interrupt mode on SPI3. I am receiving only zero in the rx callback. Why it is happening, please help.
Thanks,
- Labels:
-
SPI
-
STM32H7 Series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2022-08-12 8:47 PM
Basic general checklist
Check max spi bitrate, sometime slave is half of master
Check gpio is toggling using scope
Connect slave mosi to gnd and read 0x00, connect to vdd and read 0xFF
Check in debug Mode peripheral registers are programmed properly
I assume spi1 and spi3 use different pins and use 4 wires. If slave nss is high, slave pins are high impedence
When in debug mode, hidd spi register because the debugger will read tyem to display their value and steal the data from sw reading properly when using breakpoints on slave
Good luck!