unable to read 32kHz oscillator signal on ETR pin
Hi all,
i'm working with a STM32F469i-discovery board trying to read the external signal at 32kHz coming from an RTC module. The oscillating signal voltage is a CMOS type. I'm using TIM2_ETR input located on pin PA15 configured as follow. I'm not able to read any pulse on the pin and every time that I run the system the oscillator voltage fall to 0.3V instead of the 2.5V that I can measure when the system is not running.
I test the oscillator signal on Arduino board and I can read the right frequency just connectin the oscillator output to Arduino pin8. Thanks for the support.