2024-05-22 3:16 PM
hi guys,
I hope this message finds you well.
I am currently working with the STM32H743Eval2 evaluation board with an external nand flash memory "Micron MT29F2G16ABAEAWP" , and i'm trying to run the code provided in the firmware on the same memory but i get an I/O error. the same error when i debuged it without connecting the memory to the board. is there any way to verify if the the memory is connected to the board ? or is there anything else messing ?
/* Determine if the I/O driver initialized successfully. */
if (media_ptr -> fx_media_driver_status != FX_SUCCESS)
{
/* Return the driver error status. */
return(FX_IO_ERROR);
}
- PG9 ------> FMC_NCE//
- PD0 ------> FMC_D2//
- PD1 ------> FMC_D3//
- PD4 ------> FMC_NOE//
- PD5 ------> FMC_NWE//
- PD6 ------> FMC_NWAIT//
- PD8 ------> FMC_D13//
- PD9 ------> FMC_D14//
- PD10 ------> FMC_D15//
- PD11 ------> FMC_CLE (FMC_A16)
- PD12 ------> FMC_ALE (FMC_A17)
- PD13 ------> FMC_A18
- PD14 ------> FMC_D0//
- PD15 ------> FMC_D1//
- PE7 ------> FMC_D4//
- PE8 ------> FMC_D5//
- PE9 ------> FMC_D6//
- PE10 ------> FMC_D7//
- PE11 ------> FMC_D8//
- PE12 ------> FMC_D9//
- PE13 ------> FMC_D10//
- PE14 ------> FMC_D11//
- PE15 ------> FMC_D12 //
2024-05-22 5:08 PM
Probably going to want to start at the bus level, and interact with the memory more directly.
Use READ ID and READ PARAMETER PAGE
2024-05-23 5:55 PM
On the STM32H743 eval board, the FMC is already connected to a flash chip on the board. Won't there be a conflict?
The flying wires for high-freq signals look frightening.