2023-08-21 11:16 AM
static void MX_UART8_Init(void)
{
__HAL_RCC_UART8_CLK_ENABLE();
//__HAL_UART_CLEAR_IDLEFLAG(&huart8);
/* USER CODE BEGIN USART1_Init 0 */
/* USER CODE END USART1_Init 0 */
/* USER CODE BEGIN USART1_Init 1 */
/* USER CODE END USART1_Init 1 */
huart8.Instance = UART8;
huart8.Init.BaudRate = 9600;
huart8.Init.WordLength = UART_WORDLENGTH_8B;
huart8.Init.StopBits = UART_STOPBITS_1;
huart8.Init.Parity = UART_PARITY_NONE;
huart8.Init.Mode = UART_MODE_TX_RX;
huart8.Init.HwFlowCtl = UART_HWCONTROL_NONE;
huart8.Init.OverSampling = UART_OVERSAMPLING_16;
huart8.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE;
huart8.Init.ClockPrescaler = UART_PRESCALER_DIV1;
huart8.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT;
if (HAL_UART_Init(&huart8) != HAL_OK)
{
Error_Handler();
}
}
Solved! Go to Solution.
2023-08-23 5:39 PM
This is generating UART8 output on Pin D1 (PJ8), also blink LED1 to show it's alive and running. Should see roughly 4.8 KHz square wave
Use the .HEX, the .c file reflect's the project's primary main.c file
2023-08-21 11:38 AM
Doesn't show how the code is called, or what the signal looks like.
Probes properly grounded?
Perhaps configure PJ8 as a GPIO and drive that high/low in a manner you can review / inspect ?
Should be the only connection for PJ8, not really understanding how it go this complicated / difficult.
Are there different versions of the H747I-DISCO board? What version are you using?
2023-08-21 11:39 AM
Watch that msg has usable content. Perhaps send "UUUUU" strings?
2023-08-22 4:02 AM
" how the code is called"
not this HAL_UART_Transmit(&huart8,(uint8_t*)msg,strlen(msg),100)? en usart1 (same configution but with no pin use usb)is "beer 50 % cake 50 % etc"
run as 0V.
"high/low in a manner you can review / inspect" this mean writepin?
DK32H7H747I$AT2
2023-08-23 9:45 AM
What version of the MB1248 board?
The static state of the UART TX pin should be HIGH
I mean HAL_GPIO_WritePin() or interaction with GPIOJ->ODR and readback via GPIOJ->IDR
Check the settings in RCC, GPIO and UART8 peripherals, inspect the registers.
Anything running in the M4 core that might interfere with what the M7 core is doing?
You're checking the right pins? The code is running and not crashing or faulting?
2023-08-23 10:26 AM
MB1248-D03
After HAL_GPIO_Init(GPIOJ, &GPIO_InitStruct); I think should not add HAL_GPIO_WritePin(GPIOJ,GPIO_PIN_8,1) ?
In my debug gpioj run as
In my register D0/D1 as(i dont know its same thing o no)
which part of rcc should i check
uart 8
2023-08-23 5:39 PM
This is generating UART8 output on Pin D1 (PJ8), also blink LED1 to show it's alive and running. Should see roughly 4.8 KHz square wave
Use the .HEX, the .c file reflect's the project's primary main.c file
2023-08-24 9:56 AM
Thanks a lot i have find my problem
2023-08-25 8:05 AM
What did the problem turn out to be? Might help others in similar situations