Skip to main content
GKim.1
Visitor II
April 21, 2020
Question

UART with STM32F4xx Using USB to TTL Converter

  • April 21, 2020
  • 1 reply
  • 1266 views

I want to do UART by connecting USB to TTL converter(PN-USBTTL-FT, FTDI FT232RL) to Tx and Rx of the board pin without using the USB port of the debugger part of STM32F4xx.

The main code is as follows:

uint8_t a = 'a';
 while (1)
 {
HAL_UART_Transmit(&huart2, &a, 1, 10);
HAL_Delay(1000);
}

The debugging board's USB(download port) can receive "aaaaa ..." input every second, but it cannot receive any value from the Tx and Rx pins assigned to CubeMX.

What should I do?

This topic has been closed for replies.

1 reply

waclawek.jan
Super User
April 21, 2020

What board?

How did you connect it to the USB convertor?

Did you connect also ground?

How do you observe it?

Did you test the USB convertor with a loopback?

Can you observe the signals using oscilloscope or LA (logic analyzer)?

JW