2020-03-04 02:21 AM
hi every one
i am trying to receive data with UART in DMA and Normal mode, but after about 10 times that I receive data correctly suddenly MCU stop working
I checked every thing but I don't know what's wrong
this is my Uart and DMA configuration :
void BSP_USART1_Init(uint32_t BaudRate)
{
__HAL_RCC_USART1_CLK_ENABLE();
uart1Handle.Instance = USART1;
uart1Handle.Init.BaudRate = BaudRate;
uart1Handle.Init.WordLength = USART1_WORD_LENGTH;
uart1Handle.Init.StopBits = USART1_STOP_BITS;
uart1Handle.Init.Parity = USART1_PARITY;
uart1Handle.Init.Mode = USART1_MODE;
uart1Handle.Init.HwFlowCtl = USART1_HWCONTROL;
uart1Handle.Init.OverSampling = USART1_OVERSAMPLING;
uart1Handle.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE;
uart1Handle.Init.ClockPrescaler = UART_PRESCALER_DIV4;
uart1Handle.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT;
uart1Handle.gState = HAL_UART_STATE_RESET;
/* USART configuration */
if(HAL_UART_Init(&uart1Handle) != HAL_OK)
{
Error_Handler();
}
USART1_DMA_Init(&uart1Handle);
/* DMA1_Stream5_IRQn interrupt configuration */
HAL_NVIC_SetPriority(DMA1_Stream5_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(DMA1_Stream5_IRQn);
/* DMA1_Stream4_IRQn interrupt configuration */
HAL_NVIC_SetPriority(DMA1_Stream4_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(DMA1_Stream4_IRQn);
}
/* *
************************* USART1 DMA initialize ******************************
* */
void USART1_DMA_Init(UART_HandleTypeDef *huart)
{
/* Deinitialize the Stream for new transfer */
HAL_DMA_DeInit(&hdmaUart1Tx);
/* Enable the DMA clock */
__HAL_RCC_DMA1_CLK_ENABLE();
hdmaUart1Tx.Instance = DMA1_Stream5;
/* Configure the hdma_uartTx handle parameters */
hdmaUart1Tx.Init.Request = DMA_REQUEST_USART1_TX;
hdmaUart1Tx.Init.Direction = DMA_MEMORY_TO_PERIPH;
hdmaUart1Tx.Init.PeriphInc = DMA_PINC_DISABLE;
hdmaUart1Tx.Init.MemInc = DMA_MINC_ENABLE;
hdmaUart1Tx.Init.PeriphDataAlignment = DMA_PDATAALIGN_BYTE;
hdmaUart1Tx.Init.MemDataAlignment = DMA_MDATAALIGN_BYTE;
hdmaUart1Tx.Init.Mode = DMA_NORMAL;
hdmaUart1Tx.Init.Priority = DMA_PRIORITY_MEDIUM;
hdmaUart1Tx.Init.FIFOMode = DMA_FIFOMODE_DISABLE;
hdmaUart1Tx.Init.FIFOThreshold = DMA_FIFO_THRESHOLD_FULL;
hdmaUart1Tx.Init.MemBurst = DMA_MBURST_SINGLE;
hdmaUart1Tx.Init.PeriphBurst = DMA_PBURST_SINGLE;
/* Configure the DMA Stream */
if(HAL_DMA_Init(&hdmaUart1Tx) != HAL_OK)
{
Error_Handler();
}
/* Associate the DMA handle */
__HAL_LINKDMA(huart, hdmatx, hdmaUart1Tx);
/* Deinitialize the Stream for new transfer */
HAL_DMA_DeInit(&hdmaUart1Rx);
hdmaUart1Rx.Instance = DMA1_Stream4;
/* Configure the hdma_uartRx handle parameters */
hdmaUart1Rx.Init.Request = DMA_REQUEST_USART1_RX;
hdmaUart1Rx.Init.Direction = DMA_PERIPH_TO_MEMORY;
hdmaUart1Rx.Init.PeriphInc = DMA_PINC_DISABLE;
hdmaUart1Rx.Init.MemInc = DMA_MINC_ENABLE;
hdmaUart1Rx.Init.PeriphDataAlignment = DMA_PDATAALIGN_BYTE;
hdmaUart1Rx.Init.MemDataAlignment = DMA_MDATAALIGN_BYTE;
hdmaUart1Rx.Init.Mode = DMA_NORMAL;
hdmaUart1Rx.Init.Priority = DMA_PRIORITY_MEDIUM;
hdmaUart1Rx.Init.FIFOMode = DMA_FIFOMODE_DISABLE;
hdmaUart1Rx.Init.FIFOThreshold = DMA_FIFO_THRESHOLD_FULL;
hdmaUart1Rx.Init.MemBurst = DMA_MBURST_SINGLE;
hdmaUart1Rx.Init.PeriphBurst = DMA_PBURST_SINGLE;
/* Configure the DMA Stream */
if(HAL_DMA_Init(&hdmaUart1Rx) != HAL_OK)
{
Error_Handler();
}
/* Associate the DMA handle */
__HAL_LINKDMA(huart, hdmarx, hdmaUart1Rx);
}
/* *
*************************** DMA_IRQHandler ************************************
* */
void DMA1_Stream4_IRQHandler(void)
{
HAL_DMA_IRQHandler(uart1Handle.hdmarx);
}
void main()
{
UART_ReadBuffer(&uart1Handle, usart1_periph_buff_rx, USART1_PRIPH_BUFF_SIZE);
While(1)
{
if(uart1Handle.RxState == HAL_UART_STATE_READY)
{
memcpy(usart1_buff_rx, usart1_periph_buff_rx, USART1_PRIPH_BUFF_SIZE);
UART_ReadBuffer(&uart1Handle, usart1_periph_buff_rx, USART1_PRIPH_BUFF_SIZE);
printf("RX:");
for(int i=0; i<USART1_PRIPH_BUFF_SIZE; i++)
printf("%x ", usart1_buff_rx[i]);
printf("\r\n");
}
}
2020-03-04 02:47 AM
"Crash" is quite genuine. Be more specific! Whta does your error handler tell?
2020-03-04 03:10 AM
The exact MCU derivate and the DMA buffer addresses might be of interest, too.
2020-03-04 04:00 AM
Stop in debugger and see where it ended up. Check peripheral settings in this state also.
2020-03-04 04:40 AM
Hi every one
Thanks for your answers
by more test and debug I realize that my SAI peripheral that is set and uses DMA1 too , causes this events .
BUT I DO NOT KNOW WHY ?
I use SAI1 in DMA mode and Rx is Circular and Double buffer but Tx is just Circular.
when I receive in UART about 10 times while SAI is working , UART Rx DMA stop suddenly but DMA interrupt routine call periodically
Is there any issue in working two peripheral by DMA1 ??!!
I use these streams :
hdmaUart1Tx.Instance = DMA1_Stream5;
hdmaUart1Rx.Instance = DMA1_Stream4;
hdma_sai1_tx.Instance = DMA1_Stream1;
hdma_sai1_rx.Instance = DMA1_Stream0;
2020-03-04 05:26 AM
Did you check the fault reason in the SCB registers ?
Assuming "crash" means hardfault, or another core fault exception.
2020-03-05 01:12 AM
How can I check the fault reason in the SCB registers ?
I don't have Hardfault or any other core exception, As I mentioned above when I receive in UART about 10 times while SAI is working , UART Rx DMA stop suddenly but DMA interrupt routine call periodically
Is there any issue in working two peripheral by DMA1 ??!!
2020-03-05 02:38 AM
>>Is there any issue in working two peripheral by DMA1 ??!!
STM32H7 ?
Not that I'm aware of, multiple streams can be active concurrently
Need to make sure you use the correct memory regions that the DMA/Bus Matrix can address
Need to manage cache coherency
Be very careful invalidating memory, and the alignment there
2020-03-05 02:51 AM
> How can I check the fault reason in the SCB registers ?
With a debugger or an appropriate hardfault-handler that outputs them. If you have no hardfault, this is irrelevent.
As said your "crash" wording is ambiguous.
> As I mentioned above when I receive in UART about 10 times while SAI is working , UART Rx DMA stop suddenly but DMA interrupt routine call periodically
Perhaps some UART Rx error condition. Like a bus contention caused by other DMA, and an induced UART Rx overflow ?
2020-04-17 04:40 AM
Have you seen the newest erreta entry? Only for V rev. with UART and DMA in combination!