2018-09-08 12:44 PM
Once a while my Error_Callback() of the UART DMA RX/TX is triggered and I can't make sense out of it.
In the HAL_UART_ErrorCallback the values are
HAL_UART_GetState(huart) == 32 // HAL_UART_STATE_BUSY_RX
HAL_UART_GetError(huart) == 16 // HAL_UART_ERROR_DMA
huart->hdmarx->ErrorCode == 0 // NONE
huart->hdmatx->ErrorCode == 2 // HAL_DMA_ERROR_FE means fifo error
Okay, so it is a FIFO error. I am not using FIFO. Any ideas?
hdma_usart2_tx.Instance = DMA1_Stream6;
hdma_usart2_tx.Init.Channel = DMA_CHANNEL_4;
hdma_usart2_tx.Init.Direction = DMA_MEMORY_TO_PERIPH;
hdma_usart2_tx.Init.PeriphInc = DMA_PINC_DISABLE;
hdma_usart2_tx.Init.MemInc = DMA_MINC_ENABLE;
hdma_usart2_tx.Init.PeriphDataAlignment = DMA_PDATAALIGN_BYTE;
hdma_usart2_tx.Init.MemDataAlignment = DMA_MDATAALIGN_BYTE;
hdma_usart2_tx.Init.Mode = DMA_NORMAL;
hdma_usart2_tx.Init.Priority = DMA_PRIORITY_VERY_HIGH;
hdma_usart2_tx.Init.FIFOMode = DMA_FIFOMODE_DISABLE;
hdma_usart2_tx.Init.FIFOThreshold = DMA_FIFO_THRESHOLD_FULL;
hdma_usart2_tx.Init.MemBurst = DMA_MBURST_INC4;
hdma_usart2_tx.Init.PeriphBurst = DMA_PBURST_INC4;
if (HAL_DMA_Init(&hdma_usart2_tx) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}
__HAL_LINKDMA(huart, hdmatx, hdma_usart2_tx);
Also I make sure that I do not call a transmit as long as the HAL_UART_TxCpltCallback() was not called and all transmits are in the main loop, not within an interrupt or callback.
2018-09-09 2:50 AM
This is a recurring question for years.
For explanation, see AN4031, chapter 4.3 Software sequence to enable DMA.
Simply ignore the error - if FIFO is not enabled, it's benign. The real solution is not to enable the FIFO error interrupt when DMA is in Direct mode; but that's probably on Cube's authors.
I don't Cube/CubeMX.
JW
2018-09-09 9:37 AM
Okay. Is there any side effect when using DMA on four UARTs (2 RX+TX, 1 TX and 1 RX)? I have the feeling that I experience packet loss when these errors happen. At least I cannot get some parts working, currently trying to figure out if the problem is my code or the interaction with the remote device.
I expect DMA for UARTs, especially if the use 38400 and 115200 baud is essentially side effect free. Correct or wrong?
2018-09-09 10:41 AM
Race conditions
Reentrant behaviour
Failures in exit paths, and response to error conditions
2018-09-09 11:57 AM
:face_screaming_in_fear:
I hate micro controllers. ;)