cancel
Showing results for 
Search instead for 
Did you mean: 

UART DMA Rx STM32H745 with LL

veera1
Associate II

Hello,

I have tried implement UART Driver only with LL Library. I'm using Nucleo-H745ZIQ. Reception through DMA is not happening. Data is not getting copied to the buffer. MPU Also Configured. I'm attaching the code. Hope DMA Configuration for Rx is ok. Please have a look and correct me if I'm wrong. Please let me know if any modifications needed

/* Includes */
#include "main.h"
#include <string.h>
 
/* Private function prototypes */
void SystemClock_Config(void);
static void MPU_Config(void);
 
/* USART related functions */
void usart_init(void);
void usart_rx_check(void);
void usart_process_data(const void* data, size_t len);
void usart_send_string(const char* str);
 
#define ARRAY_LEN(x)            (sizeof(x) / sizeof((x)[0]))
 
char usart_rx_dma_buffer[10];
 
int main(void) 
{
	
    	/* MCU Configuration */
	MPU_Config();
	
    	/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
    	LL_APB4_GRP1_EnableClock(LL_APB4_GRP1_PERIPH_SYSCFG);
	
    	NVIC_SetPriorityGrouping(NVIC_PRIORITYGROUP_4);
	
    	/* Configure the system clock */
    	SystemClock_Config();
	
    	/* Initialize all configured peripherals */
    	usart_init();
    	usart_send_string("DMA HT & TC + USART IDLE LINE interrupts\r\n");
    	//usart_send_string("Start sending data to STM32\r\n");
	
    	/* Infinite loop */
    	while (1)
	{
			
   	}
}
 
 
void usart_init(void) 
{
    	LL_USART_InitTypeDef USART_InitStruct = {0};
    	LL_GPIO_InitTypeDef GPIO_InitStruct = {0};
	
	LL_RCC_SetUSARTClockSource(LL_RCC_USART16_CLKSOURCE_PCLK2);
	
    	/* Peripheral clock enable */
    	LL_APB2_GRP1_EnableClock(LL_APB2_GRP1_PERIPH_USART1);
	LL_AHB4_GRP1_EnableClock(LL_AHB4_GRP1_PERIPH_GPIOB);
	
	/**USART1 GPIO Configuration
	PB14   ------> USART1_TX
	PB15   ------> USART1_RX
	*/
	
    	GPIO_InitStruct.Pin = LL_GPIO_PIN_14|LL_GPIO_PIN_15;
	GPIO_InitStruct.Mode = LL_GPIO_MODE_ALTERNATE;
	GPIO_InitStruct.Speed = LL_GPIO_SPEED_FREQ_HIGH;
	GPIO_InitStruct.OutputType = LL_GPIO_OUTPUT_PUSHPULL;
	GPIO_InitStruct.Pull = LL_GPIO_PULL_NO;
	GPIO_InitStruct.Alternate = LL_GPIO_AF_4;
	LL_GPIO_Init(GPIOB, &GPIO_InitStruct);
	
    	/* USART1 DMA Init for RX */
	
    	LL_DMA_SetPeriphRequest(DMA1, LL_DMA_STREAM_0, LL_DMAMUX1_REQ_USART1_RX);
	
	LL_DMA_SetDataTransferDirection(DMA1, LL_DMA_STREAM_0, LL_DMA_DIRECTION_PERIPH_TO_MEMORY);
	LL_DMA_SetStreamPriorityLevel(DMA1, LL_DMA_STREAM_0, LL_DMA_PRIORITY_HIGH);
	LL_DMA_SetMode(DMA1, LL_DMA_STREAM_0, LL_DMA_MODE_CIRCULAR);
	LL_DMA_SetPeriphIncMode(DMA1, LL_DMA_STREAM_0, LL_DMA_PERIPH_NOINCREMENT);
	LL_DMA_SetMemoryIncMode(DMA1, LL_DMA_STREAM_0, LL_DMA_MEMORY_INCREMENT);
	LL_DMA_SetPeriphSize(DMA1, LL_DMA_STREAM_0, LL_DMA_PDATAALIGN_BYTE);
	LL_DMA_SetMemorySize(DMA1, LL_DMA_STREAM_0, LL_DMA_MDATAALIGN_BYTE);
	LL_DMA_DisableFifoMode(DMA1, LL_DMA_STREAM_0);
	
    	LL_DMA_SetPeriphAddress(DMA1, LL_DMA_STREAM_0, LL_USART_DMA_GetRegAddr(USART1, LL_USART_DMA_REG_DATA_RECEIVE ));
    	LL_DMA_SetMemoryAddress(DMA1, LL_DMA_STREAM_0, (uint32_t)usart_rx_dma_buffer);
    	LL_DMA_SetDataLength(DMA1, LL_DMA_STREAM_0, ARRAY_LEN(usart_rx_dma_buffer));
	
	/* DMA interrupt init */
	NVIC_SetPriority(DMA1_Stream0_IRQn, NVIC_EncodePriority(NVIC_GetPriorityGrouping(), 0, 0));
	NVIC_EnableIRQ(DMA1_Stream0_IRQn);
	    
	/* USART configuration */
	USART_InitStruct.BaudRate = 115200;
	USART_InitStruct.DataWidth = LL_USART_DATAWIDTH_8B;
	USART_InitStruct.StopBits = LL_USART_STOPBITS_1;
	USART_InitStruct.Parity = LL_USART_PARITY_NONE;
	USART_InitStruct.TransferDirection = LL_USART_DIRECTION_TX_RX;
	USART_InitStruct.HardwareFlowControl = LL_USART_HWCONTROL_NONE;
	USART_InitStruct.OverSampling = LL_USART_OVERSAMPLING_16;
	LL_USART_Init(USART1, &USART_InitStruct);
	    
	LL_USART_ConfigAsyncMode(USART1);
	LL_USART_EnableDMAReq_RX(USART1);
	LL_USART_EnableIT_IDLE(USART1);
	    
	/* USART interrupt */
	NVIC_SetPriority(USART1_IRQn, NVIC_EncodePriority(NVIC_GetPriorityGrouping(), 0, 0));
	NVIC_EnableIRQ(USART1_IRQn);
	    
	/* Enable USART and DMA */
	LL_USART_Enable(USART1);
	LL_DMA_EnableStream(DMA1, LL_DMA_STREAM_0);
	
	/* Enable HT & TC interrupts */
	//LL_DMA_EnableIT_HT(DMA1, LL_DMA_STREAM_0);
	LL_DMA_EnableIT_TC(DMA1, LL_DMA_STREAM_0);
	LL_DMA_EnableIT_TE(DMA1, LL_DMA_STREAM_0);
}
 
void DMA1_Stream0_IRQHandler(void) 
{
	/* Check transfer-complete interrupt */
	if(LL_DMA_IsActiveFlag_TC0(DMA1)) {
	    LL_DMA_ClearFlag_TC0(DMA1);             /* Clear transfer complete flag */
	    usart_rx_check();                       /* Check for data to process */
	}
	/* Check transfer-error interrupt */
	if (LL_DMA_IsActiveFlag_TE0(DMA1)) {
	    LL_DMA_ClearFlag_TC0(DMA1);             /* Clear transfer complete flag */
	    usart_rx_check();                       /* Check for data to process */
	}
	  
    /* Implement other events when needed */
}
 
void USART1_IRQHandler(void) 
{
	/* Check for IDLE line interrupt */
	if (LL_USART_IsEnabledIT_IDLE(USART1) && LL_USART_IsActiveFlag_IDLE(USART1)) {
		LL_USART_ClearFlag_IDLE(USART1);        /* Clear IDLE line flag */
		usart_rx_check();                       /* Check for data to process */
	}
}
 
void SystemClock_Config(void) 
{
	
    	/* Configure flash latency */
    	LL_FLASH_SetLatency(LL_FLASH_LATENCY_4);
	while(LL_FLASH_GetLatency()!= LL_FLASH_LATENCY_4)
	{
	}
	LL_PWR_ConfigSupply(LL_PWR_DIRECT_SMPS_SUPPLY);
	LL_PWR_SetRegulVoltageScaling(LL_PWR_REGU_VOLTAGE_SCALE0);
	LL_RCC_HSE_Enable();
	
	/* Wait till HSE is ready */
	while(LL_RCC_HSE_IsReady() != 1)
	{
		
	}
	LL_RCC_PLL_SetSource(LL_RCC_PLLSOURCE_HSE);
	LL_RCC_PLL1P_Enable();
	LL_RCC_PLL1_SetVCOInputRange(LL_RCC_PLLINPUTRANGE_8_16);
	LL_RCC_PLL1_SetVCOOutputRange(LL_RCC_PLLVCORANGE_WIDE);
	LL_RCC_PLL1_SetM(1);
	LL_RCC_PLL1_SetN(120);
	LL_RCC_PLL1_SetP(2);
	LL_RCC_PLL1_SetQ(2);
	LL_RCC_PLL1_SetR(2);
	LL_RCC_PLL1_Enable();
	
	/* Wait till PLL is ready */
	while(LL_RCC_PLL1_IsReady() != 1)
	{
	}
	
	/* Intermediate AHB prescaler 2 when target frequency clock is higher than 80 MHz */
	LL_RCC_SetAHBPrescaler(LL_RCC_AHB_DIV_2);
	
	LL_RCC_SetSysClkSource(LL_RCC_SYS_CLKSOURCE_PLL1);
	
	/* Wait till System clock is ready */
	while(LL_RCC_GetSysClkSource() != LL_RCC_SYS_CLKSOURCE_STATUS_PLL1)
	{
		
	}
	LL_RCC_SetSysPrescaler(LL_RCC_SYSCLK_DIV_1);
	LL_RCC_SetAHBPrescaler(LL_RCC_AHB_DIV_2);
	LL_RCC_SetAPB1Prescaler(LL_RCC_APB1_DIV_2);
	LL_RCC_SetAPB2Prescaler(LL_RCC_APB2_DIV_2);
	LL_RCC_SetAPB3Prescaler(LL_RCC_APB3_DIV_2);
	LL_RCC_SetAPB4Prescaler(LL_RCC_APB4_DIV_2);
	
	LL_Init1msTick(480000000);
	
	LL_SetSystemCoreClock(480000000);
}
 
/** MPU Configuration **/
void MPU_Config(void)
{
	/* Disables the MPU */
	LL_MPU_Disable();
	
	// Initializes and configures the RAM Region and the memory to be protected 
  	LL_MPU_ConfigRegion(LL_MPU_REGION_NUMBER0, 0x0, 0x24000000, LL_MPU_TEX_LEVEL0|LL_MPU_REGION_SIZE_8KB|LL_MPU_REGION_FULL_ACCESS|LL_MPU_INSTRUCTION_ACCESS_ENABLE|LL_MPU_ACCESS_SHAREABLE|LL_MPU_ACCESS_CACHEABLE|LL_MPU_ACCESS_NOT_BUFFERABLE);
  	LL_MPU_EnableRegion(LL_MPU_REGION_NUMBER0);
	
  	// Initializes and configures the Flash Region and the memory to be protected
  	LL_MPU_ConfigRegion(LL_MPU_REGION_NUMBER1, 0x0, 0x08000000, LL_MPU_TEX_LEVEL0|LL_MPU_REGION_SIZE_1MB|LL_MPU_REGION_FULL_ACCESS|LL_MPU_INSTRUCTION_ACCESS_ENABLE|LL_MPU_ACCESS_NOT_SHAREABLE|LL_MPU_ACCESS_CACHEABLE|LL_MPU_ACCESS_NOT_BUFFERABLE);
  	LL_MPU_EnableRegion(LL_MPU_REGION_NUMBER1);
	
  	//Initializes and configures the FMC Region and the memory to be protected
  	LL_MPU_ConfigRegion(LL_MPU_REGION_NUMBER2, 0x0, 0x60000000, LL_MPU_TEX_LEVEL0|LL_MPU_REGION_SIZE_512MB|LL_MPU_REGION_FULL_ACCESS|LL_MPU_INSTRUCTION_ACCESS_ENABLE|LL_MPU_ACCESS_SHAREABLE|LL_MPU_ACCESS_NOT_CACHEABLE|LL_MPU_ACCESS_BUFFERABLE);
  	LL_MPU_EnableRegion(LL_MPU_REGION_NUMBER2);
	
	/* Enables the MPU */
	LL_MPU_Enable(LL_MPU_CTRL_PRIVILEGED_DEFAULT);
	
}

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
Imen.D
ST Employee

Hello @veera​ and welcome to the Community :)

Maybe it's cache issues: DMA is not working on STM32H7 devices

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen

Pay attention to where the buffer memory is situated, and that you're actively manager for cache-coherency where appropriate.

Remember also that the cache is managed on 32-byte lines, and you really want to avoid spanning lines front and back of the buffer, and other data you store/park in those regions. Those can suffer collateral damage if you're inattentive. 32-line alignment, and size multiples, are strongly suggested.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
veera1
Associate II

Thank you for answering.. I have made modifications as per the suggestions provided by you. I have placed the buffer at RAM3 which is accessible by DMA1 and I have taken care of cache management but still I'm receiving null data through the DMA. I have attached my code please have a look and suggest me what are the things I need to take care of and what else I have to do.

/* Includes */
#include "main.h"
#include <string.h>
 
/* Buffer used for reception */
/* Buffer location and size should aligned to cache line size (32 bytes) */
/***************
#if defined ( __ICCARM__ )
#pragma location = 0x38000000
#elif defined ( __CC_ARM )
uint8_t __attribute__((section (".RAM_D3"))) usart_rx_dma_buffer[BUFFER_SIZE]);
#elif defined ( __GNUC__ )
uint8_t __attribute__((section (".RAM_D3"))) usart_rx_dma_buffer[BUFFER_SIZE]);
#endif 
****************/
/* Macro to get variable aligned on 32-bytes,needed for cache maintenance purpose */
 #if defined   (__GNUC__)        /* GNU Compiler */
 #define ALIGN_32BYTES(buf)  buf __attribute__ ((aligned (32)))
 #elif defined (__ICCARM__)    /* IAR Compiler */
 #define ALIGN_32BYTES(buf) _Pragma("data_alignment=32") buf
 #elif defined   (__CC_ARM)      /* ARM Compiler */
 #define ALIGN_32BYTES(buf) __align(32) buf
 #endif
 
//length of statically allocated array
#define ARRAY_LEN(x)            (sizeof(x) / sizeof((x)[0]))
 
#define BUFFER_SIZE 			10
 
ALIGN_32BYTES(static char usart_rx_dma_buffer[BUFFER_SIZE]);
 
 
/* Private function prototypes */
void SystemClock_Config(void);
void CPU_CACHE_Enable(void);
static void MPU_Config(void);
 
/* USART related functions */
void usart_init(void);
void dma_init(void);
void usart_rx_check(void);
void usart_process_data(const void* data, size_t len);
void usart_send_string(const char* str);
 
 
int main(void) 
{
	/* Enable the CPU Cache */ 
  	CPU_CACHE_Enable();
	
    	/* MCU Configuration */
	MPU_Config();
	
    	/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
    	LL_APB4_GRP1_EnableClock(LL_APB4_GRP1_PERIPH_SYSCFG);
	
    	NVIC_SetPriorityGrouping(NVIC_PRIORITYGROUP_4);
	
    	/* Configure the system clock */
    	SystemClock_Config();
	
    	/* Initialize all configured peripherals */
    	usart_init();
	dma_init();
	
    	usart_send_string("DMA HT TC  USART IDLE LINE interrupts\r\n");
    	//usart_send_string("Start sending data to STM32\r\n");
	
    	/* Infinite loop */
    	while (1)
	{
		LL_mDelay(2000);
   	}
}
 
 
void usart_init(void) 
{
    	LL_USART_InitTypeDef USART_InitStruct = {0};
    	LL_GPIO_InitTypeDef GPIO_InitStruct = {0};
	
	LL_RCC_SetUSARTClockSource(LL_RCC_USART16_CLKSOURCE_PCLK2);
	
    	/* Peripheral clock enable */
    	LL_APB2_GRP1_EnableClock(LL_APB2_GRP1_PERIPH_USART1);
	LL_AHB4_GRP1_EnableClock(LL_AHB4_GRP1_PERIPH_GPIOB);
	
	/**USART1 GPIO Configuration
	PB14   ------> USART1_TX
	PB15   ------> USART1_RX
	*/
	
    	GPIO_InitStruct.Pin			= LL_GPIO_PIN_14|LL_GPIO_PIN_15;
	GPIO_InitStruct.Mode			= LL_GPIO_MODE_ALTERNATE;
	GPIO_InitStruct.Speed 			= LL_GPIO_SPEED_FREQ_HIGH;
	GPIO_InitStruct.OutputType 		= LL_GPIO_OUTPUT_PUSHPULL;
	GPIO_InitStruct.Pull 			= LL_GPIO_PULL_NO;
	GPIO_InitStruct.Alternate 		= LL_GPIO_AF_4;
	LL_GPIO_Init(GPIOB, &GPIO_InitStruct);
	
	/* USART configuration */
	USART_InitStruct.BaudRate 		= 115200;
	USART_InitStruct.DataWidth 		= LL_USART_DATAWIDTH_8B;
	USART_InitStruct.StopBits 		= LL_USART_STOPBITS_1;
	USART_InitStruct.Parity 		= LL_USART_PARITY_NONE;
	USART_InitStruct.TransferDirection 	= LL_USART_DIRECTION_TX_RX;
	USART_InitStruct.HardwareFlowControl 	= LL_USART_HWCONTROL_NONE;
	USART_InitStruct.OverSampling 		= LL_USART_OVERSAMPLING_16;
	LL_USART_Init(USART1, &USART_InitStruct);
	
	LL_USART_ConfigAsyncMode(USART1);
	
	/* Configure NVIC for UART and interrupts */
	NVIC_SetPriority(USART1_IRQn, NVIC_EncodePriority(NVIC_GetPriorityGrouping(), 0, 0));
	NVIC_EnableIRQ(USART1_IRQn);
	
	// Enable Idle interrupt
	LL_USART_EnableIT_IDLE(USART1);
	
	/* Enable USART */
	LL_USART_Enable(USART1);
	
	// Enable DMA Rx interrupt
	LL_USART_EnableDMAReq_RX(USART1);
	
	/* Polling USART1 initialization */
    	while (!LL_USART_IsActiveFlag_TEACK(USART1) || !LL_USART_IsActiveFlag_REACK(USART1)) {}
}
 
void dma_init(void)
{
	LL_DMA_InitTypeDef dma_initstruct = {0};
	
	/* Enable the clock of DMA1 */
  	LL_AHB1_GRP1_EnableClock(LL_AHB1_GRP1_PERIPH_DMA1);
	
	/* Configure the DMA functional parameters for Rx*/
	//Set fields of initialization structure:
	dma_initstruct.PeriphOrM2MSrcAddress  = LL_USART_DMA_GetRegAddr(USART1, LL_USART_DMA_REG_DATA_RECEIVE);
	dma_initstruct.MemoryOrM2MDstAddress  = ((uint32_t)usart_rx_dma_buffer);
	dma_initstruct.Direction              = LL_DMA_DIRECTION_PERIPH_TO_MEMORY;
	dma_initstruct.Mode                   = LL_DMA_MODE_CIRCULAR;
	dma_initstruct.PeriphOrM2MSrcIncMode  = LL_DMA_PERIPH_INCREMENT;
	dma_initstruct.MemoryOrM2MDstIncMode  = LL_DMA_MEMORY_INCREMENT;
	dma_initstruct.PeriphOrM2MSrcDataSize = LL_DMA_PDATAALIGN_BYTE;
	dma_initstruct.MemoryOrM2MDstDataSize = LL_DMA_MDATAALIGN_BYTE;
	dma_initstruct.NbData                 = BUFFER_SIZE;
	dma_initstruct.PeriphRequest          = LL_DMAMUX1_REQ_USART1_RX;
	dma_initstruct.Priority               = LL_DMA_PRIORITY_HIGH;
	dma_initstruct.FIFOMode               = LL_DMA_FIFOMODE_DISABLE;
	dma_initstruct.FIFOThreshold          = LL_DMA_FIFOTHRESHOLD_FULL;
	dma_initstruct.MemBurst               = LL_DMA_MBURST_INC4;
	dma_initstruct.PeriphBurst            = LL_DMA_PBURST_INC4;
	
	/* Initialize DMA instance according to parameters defined in initialization structure. */
	LL_DMA_Init(DMA1, LL_DMA_STREAM_0, &dma_initstruct);
	
	/* Configure NVIC for DMA transfer complete/error interrupts */
	NVIC_SetPriority(DMA1_Stream0_IRQn, NVIC_EncodePriority(NVIC_GetPriorityGrouping(), 0, 0));
	NVIC_EnableIRQ(DMA1_Stream0_IRQn);
	
	/* Enable HT, TC and TE interrupts */
	LL_DMA_EnableIT_HT(DMA1, LL_DMA_STREAM_0);
  	LL_DMA_EnableIT_TC(DMA1, LL_DMA_STREAM_0);
  	LL_DMA_EnableIT_TE(DMA1, LL_DMA_STREAM_0);
	
	/*CPU Data Cache maintenance :
      	It is recommended to invalidate the CPU Data cache after the DMA transfer.
      	As the destination buffer may be used by the CPU, this guarantees Up-to-date data when CPU accesses
      	to the destination buffer located in the AXI-SRAM (which is cacheable).
     	*/
	
     	//SCB_InvalidateDCache_by_Addr((uint32_t *) usart_rx_dma_buffer, sizeof(usart_rx_dma_buffer) );
	
	/* Start the DMA transfer */
  	LL_DMA_EnableStream(DMA1, LL_DMA_STREAM_0);
}
 
void usart_process_data(const void* data, size_t len) 
{
	const uint8_t* d = data;
	for (; len > 0; --len, ++d) 
	{
		LL_USART_TransmitData8(USART1, *d);
		
		// wait until TXE flag is raised
		while (!LL_USART_IsActiveFlag_TXE(USART1)) {}
	}
	while (!LL_USART_IsActiveFlag_TC(USART1)) {}
}
 
 
void usart_send_string(const char* str) 
{
    	usart_process_data(str, strlen(str));
}
 
 
void DMA1_Stream0_IRQHandler(void) 
{
	/* Check half-transfer complete interrupt */
    	if (LL_DMA_IsEnabledIT_HT(DMA1, LL_DMA_STREAM_0) && LL_DMA_IsActiveFlag_HT0(DMA1)) {
        	LL_DMA_ClearFlag_HT0(DMA1);             /* Clear half-transfer complete flag */
        	usart_rx_check();                       /* Check for data to process */
    	}
	/* Check transfer-complete interrupt */
	if(LL_DMA_IsActiveFlag_TC0(DMA1)) {
		LL_DMA_ClearFlag_TC0(DMA1);             /* Clear transfer complete flag */
	    	usart_rx_check();                       /* Check for data to process */
	}
	/* Check transfer-error interrupt */
	if (LL_DMA_IsActiveFlag_TE0(DMA1)) {
	    	LL_DMA_ClearFlag_TE0(DMA1);             /* Clear transfer complete flag */
	    	usart_rx_check();                       /* Check for data to process */
	}
}
 
void USART1_IRQHandler(void) 
{
	/* Check for IDLE line interrupt */
	if (LL_USART_IsEnabledIT_IDLE(USART1) && LL_USART_IsActiveFlag_IDLE(USART1)) {
		LL_USART_ClearFlag_IDLE(USART1);        /* Clear IDLE line flag */
		usart_rx_check();                       /* Check for data to process */
	}
}
 
/* CPU L1-Cache enable */
void CPU_CACHE_Enable(void)
{
	/* Enable I-Cache */
	SCB_EnableICache();
	
	/* Enable D-Cache */
      	SCB_EnableDCache();
}
 
void usart_rx_check(void) 
{	
	static size_t old_pos;
	size_t pos;
	    
	/* Calculate current position in buffer and check for new data available */
	pos = ARRAY_LEN(usart_rx_dma_buffer) - LL_DMA_GetDataLength(DMA1, LL_DMA_STREAM_0);
	if (pos != old_pos) {                       /* Check change in received data */
	    if (pos > old_pos) {                    /* Current position is over previous one */
		usart_process_data(&usart_rx_dma_buffer[old_pos], pos - old_pos);
	    } else {
		usart_process_data(&usart_rx_dma_buffer[old_pos], 
                ARRAY_LEN(usart_rx_dma_buffer) - old_pos);
		if (pos > 0) {
		    usart_process_data(&usart_rx_dma_buffer[0], pos);
		}
	    }
	    old_pos = pos;                          /* Save current position as old for next transfers */
	}
 }

Thank you for answering..

I have made modifications as per the suggestions provided by you. I have placed the buffer at RAM3 which is accessible by DMA1 and I have taken care of cache management but still I'm receiving null data through the DMA. I have attached my code please have a look and suggest me what are the things I need to take care of and what else I have to do. Code posted below as a answer please have a look