2022-06-22 01:33 AM
Hello,
I have tried implement UART Driver only with LL Library. I'm using Nucleo-H745ZIQ. Reception through DMA is not happening. Data is not getting copied to the buffer. MPU Also Configured. I'm attaching the code. Hope DMA Configuration for Rx is ok. Please have a look and correct me if I'm wrong. Please let me know if any modifications needed
/* Includes */
#include "main.h"
#include <string.h>
/* Private function prototypes */
void SystemClock_Config(void);
static void MPU_Config(void);
/* USART related functions */
void usart_init(void);
void usart_rx_check(void);
void usart_process_data(const void* data, size_t len);
void usart_send_string(const char* str);
#define ARRAY_LEN(x) (sizeof(x) / sizeof((x)[0]))
char usart_rx_dma_buffer[10];
int main(void)
{
/* MCU Configuration */
MPU_Config();
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
LL_APB4_GRP1_EnableClock(LL_APB4_GRP1_PERIPH_SYSCFG);
NVIC_SetPriorityGrouping(NVIC_PRIORITYGROUP_4);
/* Configure the system clock */
SystemClock_Config();
/* Initialize all configured peripherals */
usart_init();
usart_send_string("DMA HT & TC + USART IDLE LINE interrupts\r\n");
//usart_send_string("Start sending data to STM32\r\n");
/* Infinite loop */
while (1)
{
}
}
void usart_init(void)
{
LL_USART_InitTypeDef USART_InitStruct = {0};
LL_GPIO_InitTypeDef GPIO_InitStruct = {0};
LL_RCC_SetUSARTClockSource(LL_RCC_USART16_CLKSOURCE_PCLK2);
/* Peripheral clock enable */
LL_APB2_GRP1_EnableClock(LL_APB2_GRP1_PERIPH_USART1);
LL_AHB4_GRP1_EnableClock(LL_AHB4_GRP1_PERIPH_GPIOB);
/**USART1 GPIO Configuration
PB14 ------> USART1_TX
PB15 ------> USART1_RX
*/
GPIO_InitStruct.Pin = LL_GPIO_PIN_14|LL_GPIO_PIN_15;
GPIO_InitStruct.Mode = LL_GPIO_MODE_ALTERNATE;
GPIO_InitStruct.Speed = LL_GPIO_SPEED_FREQ_HIGH;
GPIO_InitStruct.OutputType = LL_GPIO_OUTPUT_PUSHPULL;
GPIO_InitStruct.Pull = LL_GPIO_PULL_NO;
GPIO_InitStruct.Alternate = LL_GPIO_AF_4;
LL_GPIO_Init(GPIOB, &GPIO_InitStruct);
/* USART1 DMA Init for RX */
LL_DMA_SetPeriphRequest(DMA1, LL_DMA_STREAM_0, LL_DMAMUX1_REQ_USART1_RX);
LL_DMA_SetDataTransferDirection(DMA1, LL_DMA_STREAM_0, LL_DMA_DIRECTION_PERIPH_TO_MEMORY);
LL_DMA_SetStreamPriorityLevel(DMA1, LL_DMA_STREAM_0, LL_DMA_PRIORITY_HIGH);
LL_DMA_SetMode(DMA1, LL_DMA_STREAM_0, LL_DMA_MODE_CIRCULAR);
LL_DMA_SetPeriphIncMode(DMA1, LL_DMA_STREAM_0, LL_DMA_PERIPH_NOINCREMENT);
LL_DMA_SetMemoryIncMode(DMA1, LL_DMA_STREAM_0, LL_DMA_MEMORY_INCREMENT);
LL_DMA_SetPeriphSize(DMA1, LL_DMA_STREAM_0, LL_DMA_PDATAALIGN_BYTE);
LL_DMA_SetMemorySize(DMA1, LL_DMA_STREAM_0, LL_DMA_MDATAALIGN_BYTE);
LL_DMA_DisableFifoMode(DMA1, LL_DMA_STREAM_0);
LL_DMA_SetPeriphAddress(DMA1, LL_DMA_STREAM_0, LL_USART_DMA_GetRegAddr(USART1, LL_USART_DMA_REG_DATA_RECEIVE ));
LL_DMA_SetMemoryAddress(DMA1, LL_DMA_STREAM_0, (uint32_t)usart_rx_dma_buffer);
LL_DMA_SetDataLength(DMA1, LL_DMA_STREAM_0, ARRAY_LEN(usart_rx_dma_buffer));
/* DMA interrupt init */
NVIC_SetPriority(DMA1_Stream0_IRQn, NVIC_EncodePriority(NVIC_GetPriorityGrouping(), 0, 0));
NVIC_EnableIRQ(DMA1_Stream0_IRQn);
/* USART configuration */
USART_InitStruct.BaudRate = 115200;
USART_InitStruct.DataWidth = LL_USART_DATAWIDTH_8B;
USART_InitStruct.StopBits = LL_USART_STOPBITS_1;
USART_InitStruct.Parity = LL_USART_PARITY_NONE;
USART_InitStruct.TransferDirection = LL_USART_DIRECTION_TX_RX;
USART_InitStruct.HardwareFlowControl = LL_USART_HWCONTROL_NONE;
USART_InitStruct.OverSampling = LL_USART_OVERSAMPLING_16;
LL_USART_Init(USART1, &USART_InitStruct);
LL_USART_ConfigAsyncMode(USART1);
LL_USART_EnableDMAReq_RX(USART1);
LL_USART_EnableIT_IDLE(USART1);
/* USART interrupt */
NVIC_SetPriority(USART1_IRQn, NVIC_EncodePriority(NVIC_GetPriorityGrouping(), 0, 0));
NVIC_EnableIRQ(USART1_IRQn);
/* Enable USART and DMA */
LL_USART_Enable(USART1);
LL_DMA_EnableStream(DMA1, LL_DMA_STREAM_0);
/* Enable HT & TC interrupts */
//LL_DMA_EnableIT_HT(DMA1, LL_DMA_STREAM_0);
LL_DMA_EnableIT_TC(DMA1, LL_DMA_STREAM_0);
LL_DMA_EnableIT_TE(DMA1, LL_DMA_STREAM_0);
}
void DMA1_Stream0_IRQHandler(void)
{
/* Check transfer-complete interrupt */
if(LL_DMA_IsActiveFlag_TC0(DMA1)) {
LL_DMA_ClearFlag_TC0(DMA1); /* Clear transfer complete flag */
usart_rx_check(); /* Check for data to process */
}
/* Check transfer-error interrupt */
if (LL_DMA_IsActiveFlag_TE0(DMA1)) {
LL_DMA_ClearFlag_TC0(DMA1); /* Clear transfer complete flag */
usart_rx_check(); /* Check for data to process */
}
/* Implement other events when needed */
}
void USART1_IRQHandler(void)
{
/* Check for IDLE line interrupt */
if (LL_USART_IsEnabledIT_IDLE(USART1) && LL_USART_IsActiveFlag_IDLE(USART1)) {
LL_USART_ClearFlag_IDLE(USART1); /* Clear IDLE line flag */
usart_rx_check(); /* Check for data to process */
}
}
void SystemClock_Config(void)
{
/* Configure flash latency */
LL_FLASH_SetLatency(LL_FLASH_LATENCY_4);
while(LL_FLASH_GetLatency()!= LL_FLASH_LATENCY_4)
{
}
LL_PWR_ConfigSupply(LL_PWR_DIRECT_SMPS_SUPPLY);
LL_PWR_SetRegulVoltageScaling(LL_PWR_REGU_VOLTAGE_SCALE0);
LL_RCC_HSE_Enable();
/* Wait till HSE is ready */
while(LL_RCC_HSE_IsReady() != 1)
{
}
LL_RCC_PLL_SetSource(LL_RCC_PLLSOURCE_HSE);
LL_RCC_PLL1P_Enable();
LL_RCC_PLL1_SetVCOInputRange(LL_RCC_PLLINPUTRANGE_8_16);
LL_RCC_PLL1_SetVCOOutputRange(LL_RCC_PLLVCORANGE_WIDE);
LL_RCC_PLL1_SetM(1);
LL_RCC_PLL1_SetN(120);
LL_RCC_PLL1_SetP(2);
LL_RCC_PLL1_SetQ(2);
LL_RCC_PLL1_SetR(2);
LL_RCC_PLL1_Enable();
/* Wait till PLL is ready */
while(LL_RCC_PLL1_IsReady() != 1)
{
}
/* Intermediate AHB prescaler 2 when target frequency clock is higher than 80 MHz */
LL_RCC_SetAHBPrescaler(LL_RCC_AHB_DIV_2);
LL_RCC_SetSysClkSource(LL_RCC_SYS_CLKSOURCE_PLL1);
/* Wait till System clock is ready */
while(LL_RCC_GetSysClkSource() != LL_RCC_SYS_CLKSOURCE_STATUS_PLL1)
{
}
LL_RCC_SetSysPrescaler(LL_RCC_SYSCLK_DIV_1);
LL_RCC_SetAHBPrescaler(LL_RCC_AHB_DIV_2);
LL_RCC_SetAPB1Prescaler(LL_RCC_APB1_DIV_2);
LL_RCC_SetAPB2Prescaler(LL_RCC_APB2_DIV_2);
LL_RCC_SetAPB3Prescaler(LL_RCC_APB3_DIV_2);
LL_RCC_SetAPB4Prescaler(LL_RCC_APB4_DIV_2);
LL_Init1msTick(480000000);
LL_SetSystemCoreClock(480000000);
}
/** MPU Configuration **/
void MPU_Config(void)
{
/* Disables the MPU */
LL_MPU_Disable();
// Initializes and configures the RAM Region and the memory to be protected
LL_MPU_ConfigRegion(LL_MPU_REGION_NUMBER0, 0x0, 0x24000000, LL_MPU_TEX_LEVEL0|LL_MPU_REGION_SIZE_8KB|LL_MPU_REGION_FULL_ACCESS|LL_MPU_INSTRUCTION_ACCESS_ENABLE|LL_MPU_ACCESS_SHAREABLE|LL_MPU_ACCESS_CACHEABLE|LL_MPU_ACCESS_NOT_BUFFERABLE);
LL_MPU_EnableRegion(LL_MPU_REGION_NUMBER0);
// Initializes and configures the Flash Region and the memory to be protected
LL_MPU_ConfigRegion(LL_MPU_REGION_NUMBER1, 0x0, 0x08000000, LL_MPU_TEX_LEVEL0|LL_MPU_REGION_SIZE_1MB|LL_MPU_REGION_FULL_ACCESS|LL_MPU_INSTRUCTION_ACCESS_ENABLE|LL_MPU_ACCESS_NOT_SHAREABLE|LL_MPU_ACCESS_CACHEABLE|LL_MPU_ACCESS_NOT_BUFFERABLE);
LL_MPU_EnableRegion(LL_MPU_REGION_NUMBER1);
//Initializes and configures the FMC Region and the memory to be protected
LL_MPU_ConfigRegion(LL_MPU_REGION_NUMBER2, 0x0, 0x60000000, LL_MPU_TEX_LEVEL0|LL_MPU_REGION_SIZE_512MB|LL_MPU_REGION_FULL_ACCESS|LL_MPU_INSTRUCTION_ACCESS_ENABLE|LL_MPU_ACCESS_SHAREABLE|LL_MPU_ACCESS_NOT_CACHEABLE|LL_MPU_ACCESS_BUFFERABLE);
LL_MPU_EnableRegion(LL_MPU_REGION_NUMBER2);
/* Enables the MPU */
LL_MPU_Enable(LL_MPU_CTRL_PRIVILEGED_DEFAULT);
}
2022-06-22 09:38 AM
Hello @veera and welcome to the Community 🙂
Maybe it's cache issues: DMA is not working on STM32H7 devices
Imen
2022-06-22 11:17 AM
Pay attention to where the buffer memory is situated, and that you're actively manager for cache-coherency where appropriate.
Remember also that the cache is managed on 32-byte lines, and you really want to avoid spanning lines front and back of the buffer, and other data you store/park in those regions. Those can suffer collateral damage if you're inattentive. 32-line alignment, and size multiples, are strongly suggested.
2022-06-27 10:59 PM
Thank you for answering.. I have made modifications as per the suggestions provided by you. I have placed the buffer at RAM3 which is accessible by DMA1 and I have taken care of cache management but still I'm receiving null data through the DMA. I have attached my code please have a look and suggest me what are the things I need to take care of and what else I have to do.
/* Includes */
#include "main.h"
#include <string.h>
/* Buffer used for reception */
/* Buffer location and size should aligned to cache line size (32 bytes) */
/***************
#if defined ( __ICCARM__ )
#pragma location = 0x38000000
#elif defined ( __CC_ARM )
uint8_t __attribute__((section (".RAM_D3"))) usart_rx_dma_buffer[BUFFER_SIZE]);
#elif defined ( __GNUC__ )
uint8_t __attribute__((section (".RAM_D3"))) usart_rx_dma_buffer[BUFFER_SIZE]);
#endif
****************/
/* Macro to get variable aligned on 32-bytes,needed for cache maintenance purpose */
#if defined (__GNUC__) /* GNU Compiler */
#define ALIGN_32BYTES(buf) buf __attribute__ ((aligned (32)))
#elif defined (__ICCARM__) /* IAR Compiler */
#define ALIGN_32BYTES(buf) _Pragma("data_alignment=32") buf
#elif defined (__CC_ARM) /* ARM Compiler */
#define ALIGN_32BYTES(buf) __align(32) buf
#endif
//length of statically allocated array
#define ARRAY_LEN(x) (sizeof(x) / sizeof((x)[0]))
#define BUFFER_SIZE 10
ALIGN_32BYTES(static char usart_rx_dma_buffer[BUFFER_SIZE]);
/* Private function prototypes */
void SystemClock_Config(void);
void CPU_CACHE_Enable(void);
static void MPU_Config(void);
/* USART related functions */
void usart_init(void);
void dma_init(void);
void usart_rx_check(void);
void usart_process_data(const void* data, size_t len);
void usart_send_string(const char* str);
int main(void)
{
/* Enable the CPU Cache */
CPU_CACHE_Enable();
/* MCU Configuration */
MPU_Config();
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
LL_APB4_GRP1_EnableClock(LL_APB4_GRP1_PERIPH_SYSCFG);
NVIC_SetPriorityGrouping(NVIC_PRIORITYGROUP_4);
/* Configure the system clock */
SystemClock_Config();
/* Initialize all configured peripherals */
usart_init();
dma_init();
usart_send_string("DMA HT TC USART IDLE LINE interrupts\r\n");
//usart_send_string("Start sending data to STM32\r\n");
/* Infinite loop */
while (1)
{
LL_mDelay(2000);
}
}
void usart_init(void)
{
LL_USART_InitTypeDef USART_InitStruct = {0};
LL_GPIO_InitTypeDef GPIO_InitStruct = {0};
LL_RCC_SetUSARTClockSource(LL_RCC_USART16_CLKSOURCE_PCLK2);
/* Peripheral clock enable */
LL_APB2_GRP1_EnableClock(LL_APB2_GRP1_PERIPH_USART1);
LL_AHB4_GRP1_EnableClock(LL_AHB4_GRP1_PERIPH_GPIOB);
/**USART1 GPIO Configuration
PB14 ------> USART1_TX
PB15 ------> USART1_RX
*/
GPIO_InitStruct.Pin = LL_GPIO_PIN_14|LL_GPIO_PIN_15;
GPIO_InitStruct.Mode = LL_GPIO_MODE_ALTERNATE;
GPIO_InitStruct.Speed = LL_GPIO_SPEED_FREQ_HIGH;
GPIO_InitStruct.OutputType = LL_GPIO_OUTPUT_PUSHPULL;
GPIO_InitStruct.Pull = LL_GPIO_PULL_NO;
GPIO_InitStruct.Alternate = LL_GPIO_AF_4;
LL_GPIO_Init(GPIOB, &GPIO_InitStruct);
/* USART configuration */
USART_InitStruct.BaudRate = 115200;
USART_InitStruct.DataWidth = LL_USART_DATAWIDTH_8B;
USART_InitStruct.StopBits = LL_USART_STOPBITS_1;
USART_InitStruct.Parity = LL_USART_PARITY_NONE;
USART_InitStruct.TransferDirection = LL_USART_DIRECTION_TX_RX;
USART_InitStruct.HardwareFlowControl = LL_USART_HWCONTROL_NONE;
USART_InitStruct.OverSampling = LL_USART_OVERSAMPLING_16;
LL_USART_Init(USART1, &USART_InitStruct);
LL_USART_ConfigAsyncMode(USART1);
/* Configure NVIC for UART and interrupts */
NVIC_SetPriority(USART1_IRQn, NVIC_EncodePriority(NVIC_GetPriorityGrouping(), 0, 0));
NVIC_EnableIRQ(USART1_IRQn);
// Enable Idle interrupt
LL_USART_EnableIT_IDLE(USART1);
/* Enable USART */
LL_USART_Enable(USART1);
// Enable DMA Rx interrupt
LL_USART_EnableDMAReq_RX(USART1);
/* Polling USART1 initialization */
while (!LL_USART_IsActiveFlag_TEACK(USART1) || !LL_USART_IsActiveFlag_REACK(USART1)) {}
}
void dma_init(void)
{
LL_DMA_InitTypeDef dma_initstruct = {0};
/* Enable the clock of DMA1 */
LL_AHB1_GRP1_EnableClock(LL_AHB1_GRP1_PERIPH_DMA1);
/* Configure the DMA functional parameters for Rx*/
//Set fields of initialization structure:
dma_initstruct.PeriphOrM2MSrcAddress = LL_USART_DMA_GetRegAddr(USART1, LL_USART_DMA_REG_DATA_RECEIVE);
dma_initstruct.MemoryOrM2MDstAddress = ((uint32_t)usart_rx_dma_buffer);
dma_initstruct.Direction = LL_DMA_DIRECTION_PERIPH_TO_MEMORY;
dma_initstruct.Mode = LL_DMA_MODE_CIRCULAR;
dma_initstruct.PeriphOrM2MSrcIncMode = LL_DMA_PERIPH_INCREMENT;
dma_initstruct.MemoryOrM2MDstIncMode = LL_DMA_MEMORY_INCREMENT;
dma_initstruct.PeriphOrM2MSrcDataSize = LL_DMA_PDATAALIGN_BYTE;
dma_initstruct.MemoryOrM2MDstDataSize = LL_DMA_MDATAALIGN_BYTE;
dma_initstruct.NbData = BUFFER_SIZE;
dma_initstruct.PeriphRequest = LL_DMAMUX1_REQ_USART1_RX;
dma_initstruct.Priority = LL_DMA_PRIORITY_HIGH;
dma_initstruct.FIFOMode = LL_DMA_FIFOMODE_DISABLE;
dma_initstruct.FIFOThreshold = LL_DMA_FIFOTHRESHOLD_FULL;
dma_initstruct.MemBurst = LL_DMA_MBURST_INC4;
dma_initstruct.PeriphBurst = LL_DMA_PBURST_INC4;
/* Initialize DMA instance according to parameters defined in initialization structure. */
LL_DMA_Init(DMA1, LL_DMA_STREAM_0, &dma_initstruct);
/* Configure NVIC for DMA transfer complete/error interrupts */
NVIC_SetPriority(DMA1_Stream0_IRQn, NVIC_EncodePriority(NVIC_GetPriorityGrouping(), 0, 0));
NVIC_EnableIRQ(DMA1_Stream0_IRQn);
/* Enable HT, TC and TE interrupts */
LL_DMA_EnableIT_HT(DMA1, LL_DMA_STREAM_0);
LL_DMA_EnableIT_TC(DMA1, LL_DMA_STREAM_0);
LL_DMA_EnableIT_TE(DMA1, LL_DMA_STREAM_0);
/*CPU Data Cache maintenance :
It is recommended to invalidate the CPU Data cache after the DMA transfer.
As the destination buffer may be used by the CPU, this guarantees Up-to-date data when CPU accesses
to the destination buffer located in the AXI-SRAM (which is cacheable).
*/
//SCB_InvalidateDCache_by_Addr((uint32_t *) usart_rx_dma_buffer, sizeof(usart_rx_dma_buffer) );
/* Start the DMA transfer */
LL_DMA_EnableStream(DMA1, LL_DMA_STREAM_0);
}
void usart_process_data(const void* data, size_t len)
{
const uint8_t* d = data;
for (; len > 0; --len, ++d)
{
LL_USART_TransmitData8(USART1, *d);
// wait until TXE flag is raised
while (!LL_USART_IsActiveFlag_TXE(USART1)) {}
}
while (!LL_USART_IsActiveFlag_TC(USART1)) {}
}
void usart_send_string(const char* str)
{
usart_process_data(str, strlen(str));
}
void DMA1_Stream0_IRQHandler(void)
{
/* Check half-transfer complete interrupt */
if (LL_DMA_IsEnabledIT_HT(DMA1, LL_DMA_STREAM_0) && LL_DMA_IsActiveFlag_HT0(DMA1)) {
LL_DMA_ClearFlag_HT0(DMA1); /* Clear half-transfer complete flag */
usart_rx_check(); /* Check for data to process */
}
/* Check transfer-complete interrupt */
if(LL_DMA_IsActiveFlag_TC0(DMA1)) {
LL_DMA_ClearFlag_TC0(DMA1); /* Clear transfer complete flag */
usart_rx_check(); /* Check for data to process */
}
/* Check transfer-error interrupt */
if (LL_DMA_IsActiveFlag_TE0(DMA1)) {
LL_DMA_ClearFlag_TE0(DMA1); /* Clear transfer complete flag */
usart_rx_check(); /* Check for data to process */
}
}
void USART1_IRQHandler(void)
{
/* Check for IDLE line interrupt */
if (LL_USART_IsEnabledIT_IDLE(USART1) && LL_USART_IsActiveFlag_IDLE(USART1)) {
LL_USART_ClearFlag_IDLE(USART1); /* Clear IDLE line flag */
usart_rx_check(); /* Check for data to process */
}
}
/* CPU L1-Cache enable */
void CPU_CACHE_Enable(void)
{
/* Enable I-Cache */
SCB_EnableICache();
/* Enable D-Cache */
SCB_EnableDCache();
}
void usart_rx_check(void)
{
static size_t old_pos;
size_t pos;
/* Calculate current position in buffer and check for new data available */
pos = ARRAY_LEN(usart_rx_dma_buffer) - LL_DMA_GetDataLength(DMA1, LL_DMA_STREAM_0);
if (pos != old_pos) { /* Check change in received data */
if (pos > old_pos) { /* Current position is over previous one */
usart_process_data(&usart_rx_dma_buffer[old_pos], pos - old_pos);
} else {
usart_process_data(&usart_rx_dma_buffer[old_pos],
ARRAY_LEN(usart_rx_dma_buffer) - old_pos);
if (pos > 0) {
usart_process_data(&usart_rx_dma_buffer[0], pos);
}
}
old_pos = pos; /* Save current position as old for next transfers */
}
}
2022-06-29 01:49 AM
Thank you for answering..
I have made modifications as per the suggestions provided by you. I have placed the buffer at RAM3 which is accessible by DMA1 and I have taken care of cache management but still I'm receiving null data through the DMA. I have attached my code please have a look and suggest me what are the things I need to take care of and what else I have to do. Code posted below as a answer please have a look