2025-03-06 12:28 AM - last edited on 2025-03-06 3:57 AM by mƎALLEm
Hi,
am new to STM32 and i am trying to configurate my Nucleo but i don't understand my problem i am trying to setup a basic blink code with the basic structure (serial port communication with putty , debugger stlinkv3 and communication between cores but i can manage to ger it right thank you for any help or advises)
my problem is i cant manage to setup a basic ioc files configuration for my stm32h755zi-q in the stmcubeide 1.18 i have a basic blink code using both core that work but when i try to setup whit other clock parameters configuration i cant manage to start the program (stlink v3 on the bord look like i cant connect)
Solved! Go to Solution.
2025-03-06 3:48 AM - edited 2025-03-06 3:52 AM
2025-03-06 3:51 AM - edited 2025-03-06 3:52 AM
Hello,
This was not the project I've attached previously. Your project doesn't compile.
So need to use the project I have attached and confirm if it is working or not. Then use it as a base project.
2025-03-06 4:13 AM
Reason: (255) Unknown. Please check power and cabling to target.
i again click resolve by accident but i can only run on core at the time in the debug
else the program work
2025-03-06 4:20 AM
If my project has the same issue. It's definitely a hardware issue on your board. Did you modify something on the board? a solder bridge? etc ..?
Try to connect with CubeProgrammer and tell us what do you find?
2025-03-06 4:30 AM
no i baugt it from mouser electronic and keep all the original setting, solder bridge and place foam on the under pins at the buttom to protect from shorts
i am not sure what are the thig you want me to show you are those resonable
also i try the debug usig your config and the config from Getting started with projects based on dual-core STM32H7 microcontrollers
in STM32CubeIDE
2025-03-06 4:41 AM - edited 2025-03-06 4:47 AM
Please forget about the "Getting started with projects based on dual-core STM32H7 microcontrollers" for the moment.
As you are able to connect with CubeProgrammer there is no issue in the HW.
With the project I shared, please:
1- Upload the CM7 project to the MCU.
2- Upload the CM4 project to the MCU.
3- Detach the USB cable and reconnect it again.
Do you have a toggling LEDs or not?
2025-03-06 4:54 AM
yes in the run(not debug it is working fine only debug dont work )
thank you for all your help it is really appreciated
2025-03-06 5:08 AM
Ok. So your issue is in debug and not in standalone. So it's another question.
So please accept as solution the comment that answered your question.
If you need to ask a question about the dual core debug, open a new thread in STM32CubeIDE forum board.
2025-03-06 5:16 AM
@William133467 I've changed the marking of the solution to be closest answer to your original question.
Thank you