Trying to flash code to debug a STM32L562 discovery board, erases part of the flash then stops, any suggestions?
Using a RTC example from the IDE, the STM32L562 discovery board gets to partly erasing the flash, before it stops
STMicroelectronics ST-LINK GDB server. Version 6.0.0
Copyright (c) 2021, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
InitWhile : Enabled
Waiting for debugger connection...
Debugger connected
Waiting for debugger connection...
Debugger connected
Waiting for debugger connection...
-------------------------------------------------------------------
STM32CubeProgrammer v2.9.0-RC01
-------------------------------------------------------------------
ST-LINK SN : 0030003C3137511733333639
ST-LINK FW : V3J9M3
Board : STM32L562E-DK
Voltage : 3.27V
SWD freq : 24000 KHz
Connect mode: Under Reset
Reset mode : Hardware reset
Device ID : 0x472
Revision ID : Rev Z
Device name : STM32L5xx
Flash size : 512 KBytes
Device type : MCU
Device CPU : Cortex-M33
BL Version : --
Memory Programming ...
Opening and parsing file: ST-LINK_GDB_server_a13612.srec
File : ST-LINK_GDB_server_a13612.srec
Size : 16712 Bytes
Address : 0x08000000
Erasing memory corresponding to segment 0:
Erasing internal memory sectors [0 8]
Download in Progress:
Error: Fail to write buffer in flash
Error: failed to erase memory
Error: failed to download Segment[0]
Error: failed to download the File
Shutting down...
Exit.
BUT, if i take the example code .hex for the discovery board and use the STCube Programmer, I can get the board back to life as the previous operation had erase some flash.
So the Programmer is able to read/write code to the discovery board, but the IDE can't get debug code to run.
Any thoughts?