2025-08-05 3:14 AM
Hi,
I have recently procured STM32L562E-DK Discovery kit. Having installed STM32 Cube IDE & STM32 Cube Programmer I tried to debug & run existing examples. However STLink is not getting detected on Windows 10 laptop. I have connected USB Type A to Micro B cable to CN17 connector. While the board powers up and is running default power measurement demo (out of box) I am unable to do any debugging/downloading of other example code.
I have tried using different USB cables & tried switching USB port on laptop. However there is no USB activity detected in Device manager. I have confirmed STLink driver installation & working through another STM32 board (Nucleo-64) where I am able to debug/program
Are there any switch/jumper settings on DK kit or do I need to connect USB Type C as well (already tried) to make the debugger work?
Any suggestions/inputs appreciated
Thanks
Solved! Go to Solution.
2025-08-05 4:32 AM
The CN17 connection is all you need for debugging. Is LD3 flashing red?
Sounds like you're using a power only USB cable.
2025-08-05 3:41 AM
FAQ: Possible communication failure between STLINK-V3 and some recent computers
2025-08-05 4:32 AM
The CN17 connection is all you need for debugging. Is LD3 flashing red?
Sounds like you're using a power only USB cable.
2025-08-05 11:45 PM
Thanks @Andrew Neil
2025-08-05 11:46 PM
@TDK thanks a lot, you were right, bought new cable with data capabilities & problem is solved