User Activity

Using a RTC example from the IDE, the STM32L562 discovery board gets to partly erasing the flash, before it stopsSTMicroelectronics ST-LINK GDB server. Version 6.0.0Copyright (c) 2021, STMicroelectronics. All rights reserved.Starting server with the ...
Posted on September 30, 2016 at 12:05I have an issue with a STHVDAC-253M which provides 0 to 25V dc to tune a cap for use with an antenna.Currently I can only get a steady 0v or 25V out of the  device, the DAC has a 7 bit register and anything above...