Trigger ADC1 scan using TIM1 CC1 on F410RB
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-09-20 4:08 AM
Hi,
I use STM32F410RB, and I need to trigger an ADC1 scan regular conversion every TIM1 CC1 event. I am sure that TIM1 works, because I have an interrupt that is triggered every CC1 event. I tried to configure ADC as follows:
ADC_ChannelConfTypeDef sConfig;
/* ADC Initialization */
AdcHandle.Instance = ADC1;
AdcHandle.Init.ClockPrescaler = ADC_CLOCK_SYNC_PCLK_DIV4;
AdcHandle.Init.Resolution = ADC_RESOLUTION_12B;
AdcHandle.Init.ScanConvMode = ENABLE;
AdcHandle.Init.ContinuousConvMode = DISABLE;
AdcHandle.Init.DiscontinuousConvMode = DISABLE;
AdcHandle.Init.NbrOfDiscConversion = 0;
AdcHandle.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_RISING;
AdcHandle.Init.ExternalTrigConv = ADC_EXTERNALTRIGCONV_T1_CC1;
AdcHandle.Init.DataAlign = ADC_DATAALIGN_RIGHT;
AdcHandle.Init.NbrOfConversion = 2;
AdcHandle.Init.DMAContinuousRequests = DISABLE;
AdcHandle.Init.EOCSelection = ADC_EOC_SINGLE_CONV;
HAL_ADC_Init(&AdcHandle);
/* Configure ADC3 regular channel */
sConfig.Channel = ADC_CHANNEL_0;
sConfig.Rank = 1;
sConfig.SamplingTime = ADC_SAMPLETIME_3CYCLES;
sConfig.Offset = 0;
HAL_ADC_ConfigChannel(&AdcHandle, &sConfig);
/* Configure ADC3 regular channel */
sConfig.Channel = ADC_CHANNEL_1;
sConfig.Rank = 2;
sConfig.SamplingTime = ADC_SAMPLETIME_3CYCLES;
sConfig.Offset = 0;
HAL_ADC_ConfigChannel(&AdcHandle, &sConfig);
HAL_ADC_Start_IT(&AdcHandle);
But ADC no interrupt is triggered. Which register, which bit are involved in the configuration? best regards Max #adc #timer #stm32f410rb
Note: this post was migrated and contained many threaded conversations, some content may be missing.
- Labels:
-
ADC
-
STM32F4 Series
-
TIM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-11-08 12:44 PM
Experimenting may be fun, but the primary source of information is (ought to be) the RM/DS.
If only Cube and the RM/DS came from the same universe. Of course I refer to the RM/DS in attempting to understand what Cube has emitted. It's always an adventure (on the other hand, it's easier than trying to use MSP430 peripherals, but I digress).
So you wanted to use one of the PWM modes. I don't know how are they called in the Cube parlance.
That's what I thought. I tried 'Active on match' thinking that sounded like a reasonable suspect. Didn't work. Now I'm thinking perhaps I need to reverse engineer the documentation further to figure out what other output mode configuration is required. If only there was a relevant ST example - like, say, the test code they used to qualify this functionality in test. But I fantasize.
Toggle is fine too if it fits other purposes that timer may be used for.
Toggle rather annoys me; it's a hack. It works - and isn't the ISR-based workaround described elsewhere - but it's clearly a hack.
Perhaps I can spend another hour or two and figure out what ST's documentation is trying to tell me, or what it neglects to mention.
Cheers.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-11-08 12:56 PM
[STM32Cube_FW_F4_V1.15.0]\Drivers\STM32F4xx_HAL_Driver\Inc\stm32f4xx_hal_tim.h :
/** @defgroup TIM_Output_Compare_and_PWM_modes TIM Output Compare and PWM modes
* @{ */&sharpdefine TIM_OCMODE_TIMING 0x00000000U&sharpdefine TIM_OCMODE_ACTIVE (TIM_CCMR1_OC1M_0)&sharpdefine TIM_OCMODE_INACTIVE (TIM_CCMR1_OC1M_1)&sharpdefine TIM_OCMODE_TOGGLE (TIM_CCMR1_OC1M_0 | TIM_CCMR1_OC1M_1)&sharpdefine TIM_OCMODE_PWM1 (TIM_CCMR1_OC1M_1 | TIM_CCMR1_OC1M_2)&sharpdefine TIM_OCMODE_PWM2 (TIM_CCMR1_OC1M)&sharpdefine TIM_OCMODE_FORCED_ACTIVE (TIM_CCMR1_OC1M_0 | TIM_CCMR1_OC1M_2)&sharpdefine TIM_OCMODE_FORCED_INACTIVE (TIM_CCMR1_OC1M_2)So you want TIM_OCMODE_PWM1 instead of TIM_OCMODE_TIMING .
This is the reason why I find 'libraries' superfluous. I wouldn't touch Cube with a stick. YMMV.
JW
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-11-08 1:08 PM
So you want TIM_OCMODE_PWM1 instead of TIM_OCMODE_TIMING .
Thanks. Why is this different than TIM_OCMODE_ACTIVE in terms of triggering the ADC? I'd expect one TIM1-clock width pulse at OC1REF with TIM_OCMODE_ACTIVE as long as the CCR register value is inside the up-count range of TIM1.

- « Previous
-
- 1
- 2
- Next »