Transfer Error (invalid Data) with USART1 & DMA
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-06-23 6:19 AM
Hello,
I setup USART1 using DMA with a STM32G071 & using HAL lib.
Currently, i try to send uint8_t TxBuffer[7]={0x16,0x07,0x98,0x09,0x00,0x00,1B}.
Transfert is done using HAL_UART_Transmit_DMA(&huart1, &TxBuffer[0], 7) and i have well manage the required interrupt signals because it send 7 bytes on Tx signal multiples times & not only ones;
but on the Tx Signal when i look the data transmitted by the DMA to USART, i can see the folowing data {0x16,0x07,0x98,0x03,0xD0,0x00,00}... 3 first bytes are always right but the other bytes values are always wrong...
It look like that DMA was badly configurate (wrong memory increment). but it seem right (see below):
hdma_usart1_tx.Instance = DMA1_Channel3;
hdma_usart1_tx.Init.Request = DMA_REQUEST_USART1_TX;
hdma_usart1_tx.Init.Direction = DMA_MEMORY_TO_PERIPH;
hdma_usart1_tx.Init.PeriphInc = DMA_PINC_DISABLE;
hdma_usart1_tx.Init.MemInc = DMA_MINC_ENABLE;
hdma_usart1_tx.Init.PeriphDataAlignment = DMA_PDATAALIGN_BYTE;
hdma_usart1_tx.Init.MemDataAlignment = DMA_PDATAALIGN_BYTE;
hdma_usart1_tx.Init.Mode = DMA_NORMAL;
hdma_usart1_tx.Init.Priority = DMA_PRIORITY_LOW;
Do you have any idea what it happens here?
Thanks a lot
- Labels:
-
DMA
-
STM32G0 Series
-
UART-USART
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-06-23 6:44 AM
Is this reproducible?
What's your hardware and how do you receive the data exactly?
What's the primary clock source of STM32?
JW
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-06-23 6:51 AM
Yes is it reproductible.
I use a stm32G071G8 mcu on custom PCB (i dont'use a nucleo board).
The data are sending out the MCU on a Tx Line & i check it with an Oscilloscope.
I have already Try a transfer Without DMA Using HAL_UART_Transmit(&huart1, &TxBuffer[0], 7,TIMEOUT) & it work well the data values are always correct.
I have also try to send a bigger buffer to check if the phenomena happens at the half of the buffer... but no, it always happens after 3 byte (it look more like a memory increment issue)
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-06-23 6:53 AM
I forgot I use internal clock sources with HCLK 55MHZ
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-06-23 7:58 AM
No idea.
Sounds like some FIFO-related issue (?)
Try to rewrite it as a minimal program without Cube/HAL, using direct register access.
JW