2021-01-23 11:44 PM
Is it possible to set I2C SCL and SDA pins to high and low in stm32 to read and write the EEPROM IC. If it is possible plz help me how to do that and how to generate the function to read and write the EEPROM 24c16 IC in stm32.Plz help me.
Thank you
Solved! Go to Solution.
2021-01-27 6:18 PM
Hello
It seems that Read operation or write are failed.
probably by some harware issue.
Note that pullup resistors must connected to SCL and SDA lines.
WP pin must grounded
2021-01-24 1:08 AM
Hello
HAL_I2C_Mem_Read(...) and HAL_I2C_Mem_Write(...) functions are suitable for this
eg
uint8_t b[6];// define the buffer
HAL_I2C_Mem_Read(&hi2c, 0xA0, 0x00, 1, b, 6, 100);// 24c16 read the first 6 bytes from page 0.
parameters
hi2c is the I2C structure
0xA0 is the slave address for page 0
0x00 is the adress of first byte of current page
1 is the length of the address
b is a pointer to buffer
6 is the length of pointer
100 msec is the timeout for this operation to return.. ( check the return value.)
2021-01-24 8:05 PM
Thank you.
uint8_t read_eeprom(uint16_t reg_addr)
{
uint8_t buffer[3]={reg_addr};
buffer[0]=(reg_addr>>8) & 0xFF;
buffer[1]=(reg_addr) & 0xFF;
while(HAL_I2C_IsDeviceReady(&hi2c1, (uint16_t)(0x50<<1), 3, 100)!=HAL_OK)
{
}
while(HAL_I2C_Master_Transmit(&hi2c1, (uint16_t)(0x50<<1), (uint8_t*)&buffer, 2, 100)!=HAL_OK)
{
if(HAL_I2C_GetError(&hi2c1)!=HAL_I2C_ERROR_AF)
{
Error_Handler();
}
}
while(HAL_I2C_IsDeviceReady(&hi2c1, (uint16_t)(0x50<<1), 3, 100)!=HAL_OK)
{
}
while(HAL_I2C_Master_Receive(&hi2c1, (uint16_t)(0x50<<1), (uint8_t*)buf, 1, 100)!=HAL_OK)
{
if(HAL_I2C_GetError(&hi2c1)!=HAL_I2C_ERROR_AF)
{
Error_Handler();
}
}
return buf;
}
I tried like this. Is this wrong or tell me plz what mistake I am doing here
2021-01-25 12:26 AM
You should read and understand the warnings that you get from the compiler.
2021-01-25 1:33 AM
okay
2021-01-25 3:49 AM
Hi,
As u told I used HAL_I2C_Mem_Read & HAL_I2C_Mem_Write in my function.
char buffer[3];
char d[3]={7, 5, 10};
these are the values given for d
at24_HAL_WriteBytes(&hi2c1, 0xA0, 0, &d, 3); //function call for write
at24_HAL_ReadBytes(&hi2c1, 0xA0, 1, buffer, 3); //function call for read
The values what I gave for 'd' is displaying on the live expression but that values are not storing in the buffer. If the values stored in the buffer the read operation is going to complete. Plz Can u help me what mistake I am doing.
Thank you
2021-01-25 5:18 AM
Hello
This is a working example made for this purpose.
Dont forget the pullup resisrors.
Here is the code
//#############################################################
uint8_t W_buf[6]={1,2,3,4,5,6};// define the write buffer
uint8_t R_buf[6];// define the read buffer
//This is the write function
if( HAL_I2C_Mem_Write(&hi2c1, 0xA0, 0x0000, 2, W_buf, 6, 100)!=HAL_OK)// 24c16 random rwrite at address 0.
{
;// possible error will trapped here
}
//this is the read function
if( HAL_I2C_Mem_Read(&hi2c1, 0xA0, 0x0000, 2, R_buf, 6, 100)!=HAL_OK)// 24c16 read at address 0.
{
;// possible error will trapped here
}
//#############################################################
2021-01-26 7:54 PM
Thank you soo much.
2021-01-26 9:16 PM
Hi,
Thank you sir. I tried as u told it is working but in R_buf the values are not storing. I don't know what to do. Plz help me sir.
2021-01-27 6:18 PM
Hello
It seems that Read operation or write are failed.
probably by some harware issue.
Note that pullup resistors must connected to SCL and SDA lines.
WP pin must grounded