2021-01-23 11:44 PM
Is it possible to set I2C SCL and SDA pins to high and low in stm32 to read and write the EEPROM IC. If it is possible plz help me how to do that and how to generate the function to read and write the EEPROM 24c16 IC in stm32.Plz help me.
Thank you
Solved! Go to Solution.
2021-01-27 7:53 PM
Thank you so much
okay I will check in the hardware part. A0, A1, A2, GND and WP Pins are connected to ground and SCL and SDA pins are connected to one end of pull resistors 10K and another ends are connected to VCC.