cancel
Showing results for 
Search instead for 
Did you mean: 

Using Internal Flash as Eprom at External Flash Application

Muharrem
Associate III

Hello.

I have a custom board with STM32F750 MCU which has 64KB Internal Flash. Since the MCU's internal Flash is very limited i added external flash to board. I developed 2 different projects for Internal and External Flash. Internal Project starts with Internal Flash address. It omly includes Memory mapped init and jump codes to external Flash. External Flash Project starts with External Flash address(0x90000000). Application code stores in here.

I need r/w internal or external flash's one page or sector as a eeprom. As i know, i can't write data to external memory because it is memory mapped. Can the application code(which stored at Ext Flash), write and read internal flash?

1 REPLY 1
TDK
Super User

> Can the application code(which stored at Ext Flash), write and read internal flash?

Yes. Application code can read/write flash, doesn't matter where it's at.

If you feel a post has answered your question, please click "Accept as Solution".