2019-04-01 2:57 AM
Hello.
I try timer 2 on STM32F427 and I have a problem. It ticks too quick.
Here is my system clock. I have external crystal: 25MHz
Clock I want to: 168MHz
void SystemClock_Config(void)
{
uint32_t i;
LL_FLASH_SetLatency(LL_FLASH_LATENCY_5);
if(LL_FLASH_GetLatency() != LL_FLASH_LATENCY_5){}
LL_PWR_SetRegulVoltageScaling(LL_PWR_REGU_VOLTAGE_SCALE1);
LL_PWR_DisableOverDriveMode();
LL_RCC_HSE_Enable();
/* Wait till HSE is ready */
while(LL_RCC_HSE_IsReady() != 1)
{ }
LL_PWR_EnableBkUpAccess();
LL_RCC_ForceBackupDomainReset();
LL_RCC_ReleaseBackupDomainReset();
LL_RCC_SetRTCClockSource(LL_RCC_RTC_CLKSOURCE_HSE);
LL_RCC_SetRTC_HSEPrescaler(LL_RCC_RTC_HSE_DIV_25);
LL_RCC_EnableRTC();
LL_RCC_PLL_ConfigDomain_SYS(LL_RCC_PLLSOURCE_HSE, LL_RCC_PLLM_DIV_25, 336, LL_RCC_PLLP_DIV_2);
LL_RCC_PLL_Enable();
/* Wait till PLL is ready */
while(LL_RCC_PLL_IsReady() != 1)
{ }
LL_RCC_SetAHBPrescaler(LL_RCC_SYSCLK_DIV_1);
LL_RCC_SetAPB1Prescaler(LL_RCC_APB1_DIV_4);
LL_RCC_SetAPB2Prescaler(LL_RCC_APB2_DIV_4);
LL_RCC_SetSysClkSource(LL_RCC_SYS_CLKSOURCE_PLL);
/* Wait till System clock is ready */
while(LL_RCC_GetSysClkSource() != LL_RCC_SYS_CLKSOURCE_STATUS_PLL)
{ }
LL_Init1msTick(168000000);
LL_SYSTICK_SetClkSource(LL_SYSTICK_CLKSOURCE_HCLK);
LL_SetSystemCoreClock(168000000);
LL_RCC_SetTIMPrescaler(LL_RCC_TIM_PRESCALER_TWICE);
// clock enable
LL_APB1_GRP1_EnableClock(LL_APB1_GRP1_PERIPH_PWR);
LL_APB2_GRP1_EnableClock(LL_APB2_GRP1_PERIPH_SYSCFG);
// MCU FLASH
LL_FLASH_EnablePrefetch();
// 1 msec timer
Init_Timer2();
}
And timer init is here:
void Init_Timer2(void)
{
LL_TIM_InitTypeDef TIM_InitStruct = {0};
LL_APB1_GRP1_EnableClock(LL_APB1_GRP1_PERIPH_TIM2);
// 1000 Hz, upcounting 32-bit
// Fclk = ( 84000000/4 )
// period = ( Fclk / 21000) = 1000
TIM_InitStruct.Prescaler = ((84000000/4)/1000 - 1) ; // 21000
TIM_InitStruct.CounterMode = LL_TIM_COUNTERMODE_UP;
TIM_InitStruct.Autoreload = 0xFFFFFFFF;
TIM_InitStruct.ClockDivision = LL_TIM_CLOCKDIVISION_DIV4;
TIM_InitStruct.RepetitionCounter = 0x00;
LL_TIM_Init(TIM2, &TIM_InitStruct);
LL_TIM_SetClockSource(TIM2, LL_TIM_CLOCKSOURCE_INTERNAL);
LL_TIM_SetTriggerOutput(TIM2, LL_TIM_TRGO_UPDATE);
LL_TIM_DisableMasterSlaveMode(TIM2);
LL_TIM_ClearFlag_UPDATE(TIM2);
LL_TIM_DisableIT_UPDATE(TIM2);
LL_TIM_EnableCounter(TIM2);
}
And system init is here:And I know, that tick of timer is too quick. I measured it (indicatively) 38x. Any idea, what is wrong?
2019-04-01 11:47 PM
> TIM_InitStruct.ClockDivision = LL_TIM_CLOCKDIVISION_DIV4;
This does not do what you may think it does - it is a prescaler for the clocks used in input filters.
JW
2019-04-02 11:09 PM
Yes. I found this information in datasheet.
Here is function solution:
{
LL_TIM_InitTypeDef TIM_InitStruct = {0};
LL_APB1_GRP1_EnableClock(LL_APB1_GRP1_PERIPH_TIM2);
// 1000 Hz, upcounting 32-bit
// Fclk = ( 42000000 )
// period = ( Fclk / 42000) = 1000 => 1ms
TIM_InitStruct.Prescaler = 42000 - 1;
TIM_InitStruct.CounterMode = LL_TIM_COUNTERMODE_UP;
TIM_InitStruct.Autoreload = 0xFFFFFFFF;
TIM_InitStruct.ClockDivision = LL_TIM_CLOCKDIVISION_DIV1;
LL_TIM_Init(TIM2, &TIM_InitStruct);
LL_APB1_GRP1_ForceReset(LL_APB1_GRP1_PERIPH_TIM2);
LL_APB1_GRP1_ReleaseReset(LL_APB1_GRP1_PERIPH_TIM2);
LL_TIM_Init(TIM2, &TIM_InitStruct);
LL_TIM_ClearFlag_UPDATE(TIM2);
LL_TIM_DisableIT_UPDATE(TIM2);
LL_TIM_EnableCounter(TIM2);
}