2019-11-07 2:54 AM
Hello,
I am trying to drive a piezo with complementary output from a timer. I am using TIM8_CH2 and TIM8_CH2 as control logic for my piezo command. I expect it to be complementary to increase volume of the piezo. TIM8 is configured as slave of TIM2 that generate the "melody".
I check the hardware output, but the thing is that I only have one of the two GPIO with a working PWM. The other one remains at '0'.
Is that possible to have complementary output on the same channel on the TIM8 (PJ6 and PJ7) on the STM32h750XB I am using ?
Both GPIO are configure as Alternate function AF3_TIM8, in Push-pull.
Here is the configuration code I am using :
static void BSP_Horn_Init_Timer(void)
{
/* Timer Output Compare Configuration Structure declaration */
TIM_OC_InitTypeDef sConfig;
/* Master and slave configurations */
TIM_SlaveConfigTypeDef sSlaveConfig;
TIM_MasterConfigTypeDef sMasterConfig;
uint32_t uhPrescalerValueWav;
// Configure the WAV_TIMx 4MHz timer base
WAV_TIMx_CLK_ENABLE();
WavTimHandle.Instance = WAV_TIMx;
uhPrescalerValueWav = (uint32_t) (SystemCoreClock / WAV_FREQUENCY) - 1;
WavTimHandle.Init.Period = 100;
WavTimHandle.Init.Prescaler = uhPrescalerValueWav;
WavTimHandle.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
WavTimHandle.Init.CounterMode = TIM_COUNTERMODE_UP;
if (HAL_TIM_PWM_Init(&WavTimHandle) != HAL_OK)
{
Error_Handler();
}
sConfig.OCMode = TIM_OCMODE_PWM1;
sConfig.Pulse = 50; // (WavTimHandle.Init.Period / 2)
sConfig.OCPolarity = TIM_OCPOLARITY_HIGH;
sConfig.OCNPolarity = TIM_OCNPOLARITY_HIGH;
sConfig.OCFastMode = TIM_OCFAST_DISABLE;
sConfig.OCIdleState = TIM_OCIDLESTATE_RESET;
sConfig.OCNIdleState = TIM_OCNIDLESTATE_RESET;
if (HAL_TIM_PWM_ConfigChannel(&WavTimHandle, &sConfig, TIM_CHANNEL_1) != HAL_OK)
{
Error_Handler();
}
/* Configure TIM2 as master & use the update event as Trigger Output (TRGO - ITR1) */
sMasterConfig.MasterOutputTrigger = TIM_TRGO_UPDATE;
sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_ENABLE;
if (HAL_TIMEx_MasterConfigSynchronization(&WavTimHandle, &sMasterConfig) != HAL_OK)
{
Error_Handler();
}
HAL_NVIC_SetPriority(WAV_IRQ, WAV_IRQ_PRIO, 0U);
HAL_NVIC_EnableIRQ(WAV_IRQ);
/* HORN_TIMx Configuation. */
HORN_TIMx_CLK_ENABLE();
TimHornHandle.Instance = HORN_TIMx;
TimHornHandle.Init.Prescaler = 0;
TimHornHandle.Init.Period = 10;
TimHornHandle.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
TimHornHandle.Init.CounterMode = TIM_COUNTERMODE_UP;
TimHornHandle.Init.RepetitionCounter = 0;
if (HAL_TIM_PWM_Init(&TimHornHandle) != HAL_OK)
{
Error_Handler();
}
sConfig.OCMode = TIM_OCMODE_PWM1;
sConfig.Pulse = 5;
sConfig.OCPolarity = TIM_OCPOLARITY_HIGH;
sConfig.OCNPolarity = TIM_OCNPOLARITY_LOW;
sConfig.OCFastMode = TIM_OCFAST_DISABLE;
sConfig.OCIdleState = TIM_OCIDLESTATE_RESET;
sConfig.OCNIdleState = TIM_OCNIDLESTATE_SET;
if (HAL_TIM_PWM_ConfigChannel(&TimHornHandle, &sConfig, TIM_CHANNEL_2) != HAL_OK)
{
Error_Handler();
}
/* Configure HORN_TIMx in Gated slave mode &
use the Internal Trigger 1 (ITR1) as trigger source */
sSlaveConfig.SlaveMode = TIM_SLAVEMODE_GATED;
sSlaveConfig.InputTrigger = TIM_TS_ITR1;
sSlaveConfig.TriggerPolarity = TIM_TRIGGERPOLARITY_NONINVERTED;
sSlaveConfig.TriggerPrescaler = TIM_TRIGGERPRESCALER_DIV1;
sSlaveConfig.TriggerFilter = 0;
if (HAL_TIM_SlaveConfigSynchronization(&TimHornHandle, &sSlaveConfig) != HAL_OK)
{
Error_Handler();
}
}
Solved! Go to Solution.
2019-11-07 3:00 AM
Read out and check the TIM registers' content. Did you enable CH2N in TIMx_CCER? I don't cube.
JW
2019-11-07 3:00 AM
Read out and check the TIM registers' content. Did you enable CH2N in TIMx_CCER? I don't cube.
JW
2019-11-07 4:17 AM
Hello,
Thanks for your quick reply. You're right, the TIM8->CCER->CC2NE was not enabled. I activate it manually in debug, and it works. I do not find any way yet to configure it using HAL, I will spend some times looking into it, or I will do it manually in the code apart from HAL. Thanks a lot
2019-11-07 5:09 AM
This has come up here previously and there's some HAL incantation for it, it's just that I loathe Cube so I am not really willing to remember these things.
JW