2017-02-11 11:39 AM
Hy.
I have a stm32f407vgt. I would like to use all TIM2 input compare for DMA trigger. I don't understand that the TIM2_CH4 is at two dma streams, and one of them with CH2, so how can i use all 4 channels at the same time?
Thanks,
Mate
Note: this post was migrated and contained many threaded conversations, some content may be missing.2017-02-11 2:24 PM
do you need all 4 PWM channels...?
this is easily configured inside cubeMX.
2017-02-11 2:42 PM
Yes I need all 4 channels. But I don't get it. TIM2_CH4 is at 2 streams at the same time, will there be a problem?
2017-02-11 3:15 PM
how long do you have between pulses ?
2017-02-11 3:48 PM
I am not an expert with the ST lineup, but I have been working on it for more than 12 months now.
Yes, you can use one or the other DMA if you want to.
did you want the 4 channels PWM to trigger 4 DMA streams ?
your request is not clear.
Input compare is usually externally triggered by a pin, is this what you want ?
therefore any external trigger can be set as an interrupt and the software can invoke any DMA stream...
2017-02-11 3:55 PM
I want 4 chanells input capture. I use 'Both edge mode'. When the input chanes its value, I want to save the timer value with dma. But I don't know that if
TIM2_CH4 is at 2 streams at the same time, when TIM2_CH4 input change occurs which stream will request dma, because TIM2_CH4 are in stream7 and stream6 with TIM2_CH2.
And also I don't have time for interrupt, because the change could be very fast.
2017-02-11 4:11 PM
TIM5 doesn't appear to suffer from this particular problem...
JW
2017-02-11 4:18 PM
I don't know. It depends on the user. But the maximum frequence would be 10Mhz.
2017-02-11 4:47 PM
do you know about this high resolution timer ?
http://www.st.com/en/microcontrollers/stm32f334.html?querycriteria=productId=LN1820
2017-02-11 7:37 PM
I think they all look routable
TIM2_CH1 DMA1 Stream 5 Channel 3
TIM2_CH2 DMA1 Stream 6 Channel 3
TIM2_CH3 DMA1 Stream 1 Channel 3
TIM2_CH4 DMA1 Stream 7 Channel 3